How to run Simcenter Samcef 2306 through Simcenter 3D 2306 from a mapped drive on Windows

2023-09-27T18:41:00.000-0400

Summary

This article describes how to start Simcenter Samcef 2306 through Simcenter 3D 2306 from a mapped drive on Windows.


Details

In order to run the Simcenter Samcef 2306 solvers from a mapped drive (remote drive) through Simcenter 3D 2306;
-    Open the Windows environment variables
-    Define the environment variable UGII_SAMCEF as following:
 
image.png
where:
1)  X: corresponds to the physical drive
                 Use the letter of the drive, don’t define the physical drive address

 2) Samcef_installation\Samcef\2306 corresponds to the path of the directory
                  where Simcenter Samcef 2306 is installed on the remote drive X
 
Then, calling Simcenter Samcef 2306 can be done through the following window of Simcenter 3D 2306, illustrated with an example of a Static Linear computation with Simcenter Samcef 2306 solver Asef:
 
image.png



image.png
 

Another way to call the Simcenter Samcef 2306 solvers from a mapped drive (i.e without defining the Windows environment variable UGII_SAMCEF) consists in defining the variable directly in the “Solver Parameter” window of Simcenter 3D 2306 as following:
 
image.png
 
 
 

KB Article ID# KB000122460_EN_US

Contents

SummaryDetails

Associated Components