Valor Process Preparation
Import BOM with multiple lines of Manufacturers and MPN in one cell.
2023-09-28T05:41:09.000-0400
Manufacturing Systems Solutions
Summary
BOM contains cells with multiple lines of Manufacturer and MPN.
Details
To import a BOM each information (Manufacturer, MPN) should be in its own cell. BOM which contains multi line information in one cell cannot directly be imported.
To be able to import such BOM, Excel can be used to split multiple lines in a cell into separate cells. Open the BOM in Excel Count the maximum number of lines in a cell (Manufacturers and MPN) which has to be split Insert empty columns for the split cells accordingly Select to column with multiple lines to be split From Data Tab run Text to Columns. Choose Delimited Next step select only Other as delimiter and enter CTRL+J in the entry field. Next step you may define a different destination for the cells. Click Finish.