After running a new installation, the VPL Service and VLM does not run.
This may occur only on new installations where a database has to be created.
An error message can be found in one of the Installer log files (*mip_history.txt)
C:\MentorGraphics\Install\LOGS
Create new instance: true
Going to create databse VPL MSSQL database user ValorPP
Changed database context to 'master'.
L:\MSSQL_DEFAULT\MSSQL13.MSSQLSERVER\MSSQL\DATA\VPL.mdf
L:\MSSQL_DEFAULT\MSSQL13.MSSQLSERVER\MSSQL\DATA\VPL_Log.ldf
Msg 1803, Level 16, State 1, Server SN1D6710, Line 1
The CREATE DATABASE statement failed. The primary file must be at least 100 MB to accommodate a copy of the model database.
Msg 5011, Level 14, State 5, Server SN1D6710, Line 1
Solution
Open Microsoft SQL Server Management Studio
Under Database --> System Database, right click on Model and open Properties.
Under Files change the Initial Size (MB) to 4
Click OK
Run the installation again.
After successful Installation set back the Initial Size.
![image.png](media/0EM4O000004mmAC)
Note: If the issue already happened then the VPL tables can be found under the System Databases/master. The should be removed savely.