Valor Process Preparation
ASM SIPLACE Pro Desk - Import of Gerber files fail
2023-09-11T07:07:19.000-0400
Manufacturing Systems Solutions
Summary
Valor Process Preparation exported Layers as Gerber files may fail to be imported in SIPLACE Pro Desk.
The Gerber file may be invalid - Coordinate X|Y found in line 1234 does not match with format statement of gerber file
Details
If such error is shown it is most likely that the format setting defined at the Gerber Export are incorrect. For example: Format Metric LZ 2.4. This would allow only coordinates of up to 99.9999 milimeter. If the Board or Panel is larger then the coordinates may not fit with the Format statement.
Change can be done during the Export or being saved as a default in the Customers Design Center.