Valor Process Preparation
KnS Assembly Cell - Configuration parameter PLM_ClientID
2023-09-11T07:08:21.000-0400
Manufacturing Systems Solutions
Summary
Using KnS AssemblyCell model instead of Assembleon iFlex model.
When multiple lines are defined in PLM to be able to choose the line to be used?
Details
To be able in PLM to identify which line to use, the configuration parameter PLM_ClientID can be used. Parameter should be set in the Submachines Settings of the KnS Assembly Cell machine model. Value is customer specific.