Converting-STP-to-Facet-model-using-MADPost (postprocessor)

2023-09-13T11:11:34.000-0400

Summary

A CAD model in Simcenter Madymo is often used for overlay but they can also be used to convert them to a facet surface using the MADPost tool. In this article steps required to achieve the workflow will be discussed.


Details

Step 1: Load the CAD file in MADPost 
image.png


Step2: :  Position and scale the CAD model as required (Based on the units of CAD file)
image.png

Step 3: Click on export model icon in MADPost
  image.png     
Select the parts of interests or all FE part. Once the selection is made, click on export and a .XML file will be created of the mesh.
image.png

Step 4: Load the exported model in XMADgic. The user needs to create the property and material cards and assign to the parts accordingly.
image.png

KB Article ID# KB000121964_EN_US

Contents

SummaryDetails

Associated Components