Simcenter Madymo Creating Simcenter Madymo Coupling using Coupling Assistant

2023-09-04T10:42:00.000-0400
Solver Models Workspace

Summary

In this article steps required for setting up a coupling model are briefly discussed.


Details

Step1: Once Coupling Assistant is invoked, create a new Project and assign the directory to save/load the files
image.png

Step2:  In the model tab, load the desired FE code by selecting code/version and similarly Madymo dummy model required for the analysis. Please convert the FE code units accordingly to match with the Madymo SI units.

image.png
image.png

Step 3: Input the Stop time and output time step for the analysis as required



Step 4: Position the dummy model with respect to FE model from the position tab using the Joints selector





Step 5: Input the velocity and acceleration values as required in the following tab




Step 6: In the coupling tab, create contact group for the contacts accordingly. Then create contacts between the two models by right clicking on the contacts listed and selecting new.  Similarly a constraints can be created, e.g. between the two models by selecting Madymo body and nodes from the FE code






Step 7: Generate coupling file by clicking on generate model icon 


image.png


 
 
 
 

KB Article ID# KB000121908_EN_US

Contents

SummaryDetails

Associated Components

Coupling FE Coupling Simulink Solver General Solver Installer / Licensing Solver Utilities