Simcenter Testing Solutions What's New in Simcenter Testlab 2306

2023-08-12T19:45:31.000-0400
Simcenter SCADAS Simcenter Testlab

Summary


Details


Direct YouTube link: https://www.youtube.com/watch?v=9KYNDy3FaTE


Simcenter Testlab 2306 is here!  

Simcenter Testlab 2306 numerical values are 23 for the year 2023 and 06 for the month of June. Previous release was Simcenter Testlab 2206.

*** See the PDF attached to this article (upper right) for a full description of the new features of Simcenter Testlab 2306. ***

Some highlights are listed below:

User-added image
Gain more insight with these new display features:
  • Property (DOF ID, Run, etc) curve linestyles in Simcenter Testlab Neo
  • Curve scrolling in Simcenter Testlab Neo
User-added image
Simcenter Testlab Neo curve scrolling

User-added image
New acoustic capabilities include:
User-added image
Variable amplitude order filter

User-added image
Get tough with latest durability innovations:
  • New hardware conditioning units U12E (higher bandwidth) and TC20 (thermocouple) for SCADAS RS hardware
  • Two Dimensional (2D) Time at Level calculations added to Simcenter Testlab Neo
  • Variable angles added to Critical Plane Analysis


User-added image
Newest features in vibration control:
  • Support of  SCADAS V24 cards in all vibration control modes
  • Enhancements for Multi-Input Multi-Output Shock Control


User-added image
New structural analysis features include: 
User-added image
MAC Table in Simcenter Testlab Neo

User-added image
Latest Transfer Path Analysis (TPA) techniques for:
  • Calculate blocked forces from in-situ experimental sources
  • Virtual Instrumentation to support blocked force methodology
User-added image
Virtual Instrumentation application

User-added image
Simcenter Testlab Neo added new features
User-added image
Extract RPM method in Simcenter Testlab Neo

User-added image
Download and installation: See the PDF attached to this article for a full description of the new features of Simcenter Testlab 2306.

KB Article ID# KB000121539_EN_US

Contents

SummaryDetails

Associated Components

SCADAS Durability SCADAS III SCADAS Lab SCADAS Mobile SCADAS PBN SCADAS RS Configuration App SCADAS RS Hardware SCADAS RS Recorder App SCADAS Recorder SCADAS XS