Assembly FEM Bridge Analysis in Simcenter 3D - Part 5 - Setup solution parameters

2023-08-08T15:36:20.000-0400

Summary

This tutorial shows how to go about setting up a structural analysis using an Assembly FEM in Simcenter 3D. The aim is to introduce the user to the power of Assembly FEMS and familiarize them with the approach and concepts involved.


Details

Part 5 - Setup solution parameters

Step 15: Set the Solution Parameters for the Analysis


image.png
•The menu that appears allows various solution parameters to be set. Check that:
•Solver is Simcenter Nastran
•Analysis Type is Structural
•Solution Type is SOL 101 Linear Statics
•The default settings will suffice for this analysis. If necessary, it is possible to modify these settings at a later stage in the model setup process

KB Article ID# KB000121470_EN_US

Contents

SummaryDetails

Associated Components