Simcenter Femap Thermal strain (Thermal Expansion)- Femap

2024-10-07T14:22:16.000-0400
Femap

Summary

The TEMPERATURE case control inputs for thermal strain and temperature dependent material properties in solutions are described as follows.


Details

QRG under Temperature
QRG link https://docs.sw.siemens.com/en-US/doc/289054037/PL20221116635232682.QRG/id511196




Linear Solutions


Nonlinear Solutions




Ways to define temperatures;  Material / Initial / Load


Material- 

Defined under reference temp




Initial-
Create a new load set and place this load standalone in the load set
Defined as load on nodes


Specify all nodes in the model and specify an initial temperature.
During the solution creation define this load set as initial conditions
 




Load
Defined as a body load- Under thermal Default temperature

creates a TEMPD card



 

KB Article ID# KB000121038_EN_US

Contents

SummaryDetails

Associated Components

API License Media Request Post Processing Preprocessing Satoolkit Stand Alone Solution Stress Wizard System Administration TMG Translator Analysis Translator Geometry Visq