Simcenter Femap
Femap; Solve using enterprise nastran license
2023-08-01T17:09:59.000-0400
FemapXcelerator ShareSimcenter Femap Marketing
Summary
FEMAP by default points to a desktop License type instead of Enterprise. Details on how to point to an enterprise seat of Nastran.
Details
FEMAP by default points to a desktop License type instead of Enterprise.
There are 2 Methods to using an enterprise license of Nastran.
Preferred method;
“Solvers” tab in “File, Preferences” to point to an Enterprise Simcenter Nastran executable. Analysis Set: “Linked Solver” and it will launch that Simcenter Nastran directly from Femap.
Second Method; this method will NEVER use the license provided by Femap, it can only use the Enterprise license.
Setup Nastran RCF file (inside the Femap directory) Prog=enterprise. Might also need; Auth=port@host
The RCF file could already have program=FEMAP. This needs to be changed to prog=enterprise so there is not duplicate lines in the RCF.
Location of RCF file and example shown below; Root directory of Femap-> Nastran-> Conf
API
License
Media Request
Post Processing
Preprocessing
Satoolkit
Stand Alone Solution
Stress Wizard
System Administration
TMG
Translator Analysis
Translator Geometry
Visq