Calibre How to fix error “sub: Command not found. **** DRC runs finished with exit code 1 ****"

2023-07-12T12:36:54.000-0400
Viewing & Interfaces

Summary

The article explains why the users get and how to fix error sub: Command not found. **** DRC runs finished with exit code 1 ****


Details


If the MGC_CALIBRE_VIEWER_MENU_CMDS environmental variable is set up with an old GUI drc.ci.custom file:
          % setenv 
MGC_CALIBRE_VIEWER_MENU_CMDS drc.ci.custom

and you opened the new gui with the existing runset file (runset created with the new Calibre Interactive GUI), you will most probably get the error as follows:
          bsub -I –R ….   **** DRC runs finished with exit code 1 ****






If you check your runset file after this, you will notice that one keyword was changed automatically:
From:
cmn.cmnRunControl.runWhere.value = "local"
To:
cmn.cmnRunControl.runWhere.value = "lsf"





To fix this issue you can try the following steps:
unsetenv 
MGC_CALIBRE_VIEWER_MENU_CMDS
% gvim runset_file

Edit the line to:
cmn.cmnRunControl.runWhere.value = "local"

Then rerun the job.

KB Article ID# KB000112631_EN_US

Contents

SummaryDetails

Associated Components

Calibre Interactive