Simcenter 3D Solutions Simcenter 3D Design Space Exploration - installation and setup

2023-07-03T14:39:12.000-0400
Simcenter 3D

Summary

Simcenter 3D Design Space Exploration is a scaled down version of HEEDS, tailored only to Simcenter 3D applications. This article guides you through the steps of downloading and installing the Simcenter 3D Design Space Exploration add-on.


Details

Downloading Simcenter 3D Design Space Exploration from Support Center

Use the following link to download the 2206 version of Simcenter 3D Design Space Exploration (Fig. 1):

Simcenter 3D 2206 Add-ons Downloads – Design Space Exploration

As of June 2023, version 2206 is the latest one for Design Space Exploration, also supporting Simcenter 3D 2212.

Fig. 1 Simcenter 3D 2206 Add-ons Downloads – Design Space Exploration

fig01_download.png

 

Installing Simcenter 3D Design Space Exploration

The software comes in a 7z package form and doesn’t require regular installation steps.

The 7z package can be extracted anywhere on your machine (Fig. 2).

Fig. 2 Extracting the Simcenter 3D Design Space Exploration package

fig02_install.png

 

Running Simcenter 3D Design Space Exploration

Design Space Exploration can be launched from the HEEDSMDO executable, located in the ..\Win64 directory of the installation folder:

  • Example: "C:\Apps\Siemens\Simcenter3D\SC3D_2206_DSE\Ver2022.1.0\Win64\HEEDSMDO.exe"

Upon a successful launch of Simcenter 3D Design Space Exploration, check that it uses the desired version of Simcenter 3D in the Options menu (Fig. 3).

Fig. 3 Simcenter 3D Design Space Exploration - Options

fig03_options.png

 

Documentation

Help documents for Simcenter 3D Design Space Exploration can be found in the ..\docs\en sub-directory of the installation folder (Fig. 4).

Fig. 4 Documentation files

fig04_docs.png

 

Prerequisites for Simcenter 3D Motion studies in Design Space Exploration

Both the Simcenter 3D and Simcenter 3D Motion portals can be used for running Simcenter 3D Motion studies. Regardless of the portal, for running any Motion simulations and studies through Design Space Exploration, the following system or user environment variable (Fig. 5) should be set:

  • HEEDS_SIMCENTER3D_MRRCMD=%path_to_mrr_exe%
  • where %path_to_mrr_exe% is the path towards the Motion Results Reader executable.

The Motion Results Reader executable can be found in the Simcenter 3D (or NX) installation in:

  • ..\MECH\motionsolver\MotionResultsReader.exe

Use the Motion Results Reader that comes with the version of Simcenter 3D you are planning on running through Design Space Exploration. Example:

  • HEEDS_SIMCENTER3D_MRRCMD=C:\Apps\Siemens\Simcenter3D\SC3D_2212\MECH\motionsolver\MotionResultsReader.exe

Fig. 5 Environment variables for Simcenter 3D Motion studies in Design Space Exploration

fig05_motion_envvars.png   

KB Article ID# KB000112494_EN_US

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow