End of Standard Maintenance for Simcenter Madymo Solver and Workspace 2306 (both released in June 2023) is listed below. This date represents when no further updates or fixes will be issued for the corresponding Simcenter Madymo Solver and Workspace. Also please note Critical Error Cut Off (last date to report issues for a possibility of a fix) for Simcenter Madymo Solver and Workspace 2306 is April 16th, 2024.
Simcenter release | End of Standard Maintenance |
---|---|
Simcenter Madymo Solver & Models 2306 | June 16, 2024 |
Simcenter Madymo Workspace 2306 | June 16, 2024 |
Simcenter Customer Support will continue to provide support and assistance for Simcenter Madymo release 2306. Simcenter Customer Support will attempt to duplicate any possible code defects on the revision of software the defect is reported (when available) and on the current release or revision of the product. Simcenter Customer Support will not write a Problem Report (PR) unless the problem can be duplicated in a supported version of the product. If it is found that the defect does not occur in the latest revision of the software, the customer will be asked to update their product to the current revision to correct the problem.
Sincerely, Siemens Digital Industries Software