•Double click the Bridge_Optimisation_sim part in the Simulation File View pane using the left mouse button
•Select User Defined Constraint from the Constraint Type drop-down menu in the Loads and Conditions group of the Home tab tool ribbon
•Select the faces of volume that point in the positive and negative y direction (large faces)
•Click OK
Step 13: Create the Gravity Load
•Select Gravity from the Load Type drop-down menu in the Loads and Conditions group of the Home tab tool ribbon
•Set Acceleration to 9810mm/s2
•Set Specify Vector to -ZC
•Click OK
Step 14: Create the Load at the Centre of the Bridge
•Select Force from the Load Type drop-down menu in the Loads and Conditions group of the Home tab tool ribbon
•Set Type to Magnitude and Direction
•Select the edge in the middle of the bottom face of the volume (face pointing in -Z direction)
•Set Force to 1250000N
•Set Specify Vector to -ZC
•In the Distribution section of the menu, set Method to Geometric distribution
•Click OK
Step 15: Setup the Design Objective
•Right click on the Design Objective and select New or Replace Design Objective…
•Set Name to Minimise_Mass
•Set Response Type to Total Model Weight (WEIGHT)
•Set Method to MIN
Step 16: Setup the Frozen Area
•Right click on the Design Area and select New Design Area…
•Set Name to Frozen
•Set Area Type to Frozen Area
•Enter Label to 2
•Select the bottom row of elements of the bridge volume
•Click OK
Step 17: Create the Symmetrical Manufacturing Constraint
•Right click on the Manufacturing Constraint and select New Manufacturing Constraint…
•Set Name to Symmetry
•Set Constraint Type to Planar Symmetry (SYMP)
•Select a point in the middle of the bottom edge (as indicated)
•Set Specify Vector to +X
•Click OK
Step 18: Create the Minimum Member Size Constraint
•Right click on the Manufacturing Constraint and select New Manufacturing Constraint…
•Set Name to Min_Size
•Set Constraint Type to Minimum Member Size (MINS)
•Set Minimum Member Size to 200mm
•Click OK
Step 19: Setup the Design Constraint
•Right click on the Design Constraint under the Nastopt – Statics 1 subcase and select New Advanced Design Constraint…
•Set Name to Disp_Constraint
•Click on the Create Modeling Object… icon

•Set Name to Disp_Response
•Set Label to DR
•Set Response Type to Displacement (DISP)
•Set DOF3 to On
•Select New Group