Topology optimization of a Bridge Structure - Part 2: Mesh the bridge geometry

2023-04-07T05:30:59.000-0400

Summary

In this example the process of performing a topology optimization for a simple bridge structure will be illustrated. The objective is to minimize the mass of the bridge while keeping the deflection less than 1mm. This is a 7 parts tutorial that includes the following: 1. Geometry creation - simple bridge shape 2. Mesh the bridge geometry 3. Apply material properties 4. Apply Loads and constraints 5. Setup and Run the analysis 6. Postprocessing results 7. Animate the Topology optimization iterations


Details

Part 2: Mesh the bridge geometry

Step 6: Create Mesh Mating Condition


image.png
•Select the Mesh Mating  image.png   tool in the Connections group of the Home tab tool ribbon
•Select all the faces from both solid bodies
•Click OK

Step 7: Create Mesh Controls in Top Corners

image.png
•Select the Mesh Control     tool in the Mesh group of the Home tab tool ribbon
•Set the Type to Number on Edge
•Select the edges of the corners cube as indicated
•Set Number of Elements to 1
•Click OK
Step 8: Create the Mesh

image.png
•Select the 3D Swept Mesh     tool in the Mesh group of the Home tab tool ribbon
•Set the Type to Multi Body-Infer Target
•Ensure that the Element Type is set to CHEX8
•Set Source Element Size to 100mm
•Select a face from each of the two bridge volume solids
•Click OK

This completes Topology optimization of a Bridge Structure - Part 2: Mesh the bridge geometry
Please continue with Topology optimization of a Bridge Structure - Part 3: Apply material properties

KB Article ID# KB000111478_EN_US

Contents

SummaryDetails

Associated Components