Tessent
The Parameter Default Value for a Verilog
2023-06-01T06:20:06.000-0400
Tessent Shell Flow
Summary
Does the default value have to be specified for a Verilog parameter?
Details
Specifying the parameter default value is
mandatory
for 1995, 2001, sv31a, and sv2005 formats, and it is
not mandatory
for the SV2009 format.
Below is the example module with a parameter being used:
module block #(parameter BUS_WIDTH) (
input [BUS_WIDTH-1:0] bus_data_in,
output [BUS_WIDTH-1:0] bus_data_out
);
endmodule
If the parameter default value is not specified, then the example error message below is returned:
// Error: File block.v, Line 10: Syntax error near ( ) ).
To resolve this issue there has to be a specified default value for a parameter or if the format is SV2009 the command below has to be used:
read_verilog block.v -format SV2009
KB Article ID# KB000111368_EN_US
Contents
Summary
Details
Associated Components
Tessent Shell Environment
Tessent MemoryBIST - TS
Tessent LogicBIST - TS
Tessent SSN
Tessent IJTAG
Tessent TestKompress
Tessent BoundaryScan - TS