Axisymmetric Pressure Vessel Analysis in Simcenter 3D - Part 4: Apply boundary conditions

2023-03-08T17:01:29.000-0500

Summary

In this article, a cylindrical pressure vessel will be analyzed using the axisymmetric analysis capability in Simcenter. It is Part 4 of 6 parts tutorial with the following steps: Part 1: Create pressure vessel geometry Part 2: Mesh the created pressure vessel model Part 3: Apply material properties Part 4: Apply boundary conditions Part 5: Create cylindrical coordinate system for the FEM Part 6: Analysis run and post processing


Details

Part 4: Apply boundary conditions on Pressure Vessel FEM model

Step 13: Create the Pressure Load

image.png

image.png
•Double click the Pressure_Vessel_sim1 part in the Simulation File View pane using the left mouse button
•Select Pressure from the Load Type drop-down menu in the Loads and Conditions group of the Home tab tool ribbon
•Set the Normal Pressure to 1MPa
•Select all the edges on the inner surface of the vessel as shown and click OK

Step 14: Constrain the Pressure Vessel

image.png
image.png
•Select User Defined Constraint from the Constraint Type drop-down menu in the Loads and Conditions group of the Home tab tool ribbon
•Set DOF1 to Fixed
•Select the two edges highlighted in the image below

KB Article ID# KB000073782_EN_US

Contents

SummaryDetails

Associated Components