Tanner Custom IC Tools
Create an .assert warning for dc operating point for transistor small-signal params in T-Spice
2023-02-10T08:26:40.000-0500
Tanner EDA
Summary
How to create a .assert warning for small-signal parameters when v(M1.vds)-v(M1.vdssat) > 300mv (T-SPICE)
Details
For specific transistors, you could use the expr part of .ASSERT. If you want to do it for all MOSFETs, that will be more involved. If you open the OpAmp design (TB_OpAmp_DC - TSP_DC) from the Shipping Files, then you can add the following to the additional SPICE commands: