Quick AMESim installation guide for Window and Linux System
2022-12-16T04:46:56.000-0500
Summary
There are multiple scenarios that may exist when you decide to install AMESim. We will walk through all the scenarios so that you can directly go to the scenario, which is more applicable to you.
Details
Installation of AMESim is depending on your requirements. It can be based on your operating system.
Window machine
Linux machine
Once, your operating system is fixed, then there will be below two scenario
Scenario 1 - Node lock license
You need to install AMESim and RLM license server on the same machine for which the license is issued.
Scenario 2 - Floating license
Wanted to access AMESim on the server machine for which the license is issued
Install AMESim and license manager on the server machine. Only install AMESim on the client machine.
Wanted to access AMESim only on the client machine -
Install the RLM license server on the server machine
Install AMESim Only AMESim on all client machines.
Once, you choose your scenario, then, you can directly go to the valid section of the below article
Wanted to access AMESim on the server machine for which the license is issued -
Install AMESim on Server and client machine - You can check the below video toknow about the AMESim installation process. Watch the below video for the first 10 minutes.
Install and configure the RLM license manager on the server machine only - Watch the below video for the first 8 min to know about RLM license manager installation Watch the below video from 8 min to end to configure your license file on the server and client machine
Wanted to access AMESim only on the client machine-
Install and configure the RLM license manager on the server machine only - Watch the below video for the first 8 min to know about RLM license manager installation & watch the same below video from 8 min to the end to configure your license file on the server and client machine.
Linux machine - Please note that in this case as well all the above three scenarios exist. In this case, as well, we have to install AMESim and license server manager on the applicable server or client machine. There will not be any change in this case.
Installation & license configuration is a bit different for Linux machines. Watch the below video related to AMESim installation on a Linux machine & refer to this article on our support portal.
If, you are still not able to access the license by the above method, then, generate the diagnosis report and send it to our support engineer by raising the support case at thislink. Please follow the below process to generate a diagnostic report. Generate rlmdiag.txt file on server machine-
It will generate therlmdiag.txtfile at the path given at the output location.
Send the rlmdiag.txtfile to me.
Generate RLMLOG.txt file on server machine-
Click on the Status tab on the left side. It will open the main server page. On the right side, you will see the path for the debug file log. Here, you can see theRLMLOG.txtfile.
Please also click on System Info Tab and send me the snap of the right side window.
The below articles can also help in the installation process. Please visit the below VIDEO articles.
CLICK HERE to know about RLM License manager installation & license configuration for Simcenter AMESim CLICK HEREto know about “Installation of Simcenter AMESim & RLM license configuration on Window 10 machine”. CLICK HERE to know How to Install & Open multiple AMESim versions on the same Window machine CLICK HERE to know about How to Install Simcenter AMESim & How to configure the Simcenter AMESim RLM license on the Linux/Ubuntu Machine.