Zel X
Is a Guest with full access only able to Mark up and Prepare projects for AR?
2023-01-12T21:20:27.000-0500
COLLABORATION
Summary
Is a Guest with full access only able to Mark up and Prepare projects for AR?
Details
Guests are invited by Members to collaborate on projects but do not require a license within the member’s account. As such, Guests without a subscription have reduced capabilities. When a Guest hovers over a command to which they don’t have access, the system will display a Not Available symbol (circle with a slash thru it). Guests can only view and edit tasks as assigned to them.