Hydrostatic pressure load in FEMAP

2023-11-10T20:42:17.000-0500

Summary

This is the processes to define a hydrostatic pressure load in Femap


Details

Create a Coordinate system at the top of the fluid level. Model->Coord Sys.
In my example I am defining Y in the direction of the depth.  Zero Y will represent the top fluid level.


Create an equation data surface. Tools->Data Surface Editor


Enter in the following equation.

Link to the Correct coordinate system.
Define the equation as listed above.   !y calls the distance in Y in the coordinate system specified. 

Density = 0.036 lbm/in^3
Gravity= 386 in/s^2
Height=Variable in
Be careful with units.  Make sure you are using consistent units. To get consistent units in my case I needed to divide by 386 in / s^2
Results in lbf/in^2
 

KB Article ID# KB000065646_EN_US

Contents

SummaryDetails

Associated Components