Simcenter Nastran Continuation Characters and Additional Flexibility in Usage.

2022-08-30T15:43:15.000-0400

Summary

The Quick Reference Guide provides format rules and examples for continuation characters and lines. The purpose of this FAQ is to provide additional information.


Details

The Quick Reference Guide states in part as follows:


Small Field Continuation Format 1:

You can enter + or * in the last field of a line and + at the beginning of the next line.

Small Field Continuation Format 2:
 

You can simply leave the continuation fields blank.


Small Field Continuation Format 3:

You can enter a unique character string in the last field of a line, then a continuation line begins with the same character string.

However it is noted that a combination of the above may be possible.

For example you can simply leave the continuation fields blank in the last field of a line and + at the beginning of the next line.

Other combinations may be possible.

Reference: IR # 10391156

KB Article ID# KB000054169_EN_US

Contents

SummaryDetails

Associated Components