Simcenter Amesim Selected compiler could not be detected

2023-01-18T09:59:19.000-0500
Simcenter Amesim Automation Connect Simcenter System Simulation Client for Git Simcenter Amesim Teamcenter Share

Summary

This article describes how to handle the issue of Amesim not detecting an installed compiler.


Details

By default, Simcenter Amesim comes in package with GNU GCC (64-bit) compiler. It can however be noticed that there are other available options like Intel C++ (64-bit). When selecting that compiler however, you may notice a following message:

This may indicate two issues:
  1. Compiler is not installed & setup properly
  2. Simcenter Amesim cannot detect the compiler
If it is the second option, please go to your install directory (for example):
C:\Program Files\Simcenter\2022.1\Amesim\misc
In that directory find the file iclvars_template.bat

When you open it, a procedure to setup a compiler will show:

Follow those steps in order to ensure that compiler will be detected by the Simcenter Amesim.
 

KB Article ID# KB000054128_EN_US

Contents

SummaryDetails

Associated Components

Amesim Automation Connect