NX Mold Connect What type of DFM analysis is available in NX Mold Connect?

2022-06-01T11:40:13.000-0400
Collaboration

Summary

This article explains what type of DFM analysis is available in NX Mold Connect?


Details

The following analysis types are available in NX Mold Connect: 
Analyze Part Geometry: Draft, undercut, cavity, and core region analysis. 
Wall Thickness: Analysis to identify wall thickness throughout the part. 
Mold Filling Advisor: Finds optimal gate locations and length/thickness ratio, sink marks, and cooling time analysis. 
Feature Recognition: Finds critical features, such as ribs, undercuts, and openings. 




If you have any questions or issues not addressed by this article, please work with the Support Engineer assigned to your Support Case – or if you have not yet reached out to our Technical Support team you can do so via Siemens Software Support Center: Open a Support Case.  
 

KB Article ID# KB000049600_EN_US

Contents

SummaryDetails

Associated Components

Collaboration