In order to understand the output provided by a Force Report, we can consider a very simple scenario:

where a cubic body is interacting with a water current travelling at a constant velocity,
Vx, and includes gravity,
g.
Under these conditions, there will be two main forces acting on the body: the fluid force due to the relative motion between the cube and the fluid, and the hydrostatic force due to the gravity.

If in Simcenter STAR-CCM+ we define a Velocity Vector [5,0,0} m/s at the inlet, and, at the end of the run, we set a Force Report (where, for simplicity we do not include the viscous contribution) to compute the X component of the Force acting on the faces -X and +X of the body, we get:
01_ForceReport(X_component) = 9610.9 N
If we define a new Force Report that, this time, computes the X component of the Force acting only on the face -X, we get:
02_ForceReport(X_componet)@-X = 31713.5 N.
What this the reason of this difference?
The report 01_ForceReport(X_component) computes the sum of all the forces acting on the faces -X and +X.

The hydrostatic contributions to the force on these two faces are balanced, and the total hydrostatic force results null.
The report 02_ForceReport(X_componet)@-X, instead, takes into account only the forces acting on face -X on which the hydrostatic contribution is no more balanced by the presence of the opposite face, +X:
What is the physical meaning of this report?
If the hydrostatic pressure is properly defined, this report returns the real force acting on the -X face of the body.
Looking at the definition of the hydrostatic pressure:
it is evident that the hydrostatic force (and so the Force Report computed on a not-closed surface) strongly depends on the reference altitude, h0.
This highlights the important conclusions below:
- A force report computed on a closed surface always returns the total force that a fluid in movement exerts on a body;
- A force report computed on an unclosed surface returns the total force that a fluid exerts, only if the reference altitude is correctly set.
see also:
Working Pressure in case of Viscous Flow simulationSimcenter STAR-CCM+ Documentation Sections:
Post-Processing > Reporting Results > Specific Reports > Force