Simcenter 3D Solutions Motion Object Already Exists within Discrete Drivetrain Element

2022-08-02T18:05:35.000-0400
Simcenter 3D

Summary

The article walks through the source and solution of a common error when creating a discrete drivetrain element. This error says "A Motion object already exists with this name" and occurs when trying to hit OK on the element dialog.


Details

Problem:
When creating a discrete drivetrain element, an error appears when trying to hit the “OK” or “Apply” buttons that says, “A Motion object already exists with this name”. This can occur even if the discrete drivetrain element has a unique name.

 
Solution:
The discrete drivetrain element contains multiple motion objects that must all have unique names. There are two opportunities in the discrete drivetrain element creation to create additional motion objects that can have conflicting names. The first is in the Layout Elements section when naming the individual layout elements. Although these are required to be associated with a motion body, it is important to give these elements a unique name.
 

The second common source of this error is in the Replicating Element section. Ensure that each replicating element that is defined does not share a name with any other motion object. (NOTE: the names here are NOT case sensitive).

KB Article ID# KB000049003_EN_US

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow