Simcenter 3D Solutions Motion system mass, CG

2024-02-21T14:06:46.000-0500
Simcenter 3D

Summary

How can I find out the mass of the total Motion model? How can I find the center of gravity, CG, of the entire system?


Details

Starting with Simcenter 3D 2021.2, it is possible to plot the mass of the whole system in a Motion simulation.
This value can be found by selecting the solution in Motion Navigator, expanding the XY Result View, then plotting the system:mass element.

image.png

In a similar fashion, the coordinates of the center of gravity can be plotted using the following System variables:
image.png

Note that for dynamics analyses, since the mechanism (system) is in motion, the X, Y, Z coordinates will change.
The value of these variables at t=0 represent the initial position of the CG.

KB Article ID# KB000048519_EN_US

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow