Why can't I see files in SaaS application that were previously there?

2023-10-01T23:19:10.000-0500

Summary

This article explains why files may appear to be missing in a SaaS application.


Details

SaaS applications allow Projects to be shared, which includes the ability for other users to edit and delete files within the project. Since all files associated with the assembly file (i.e. ASM) must be uploaded in order to View & Markup, if a file is missing it will need to be located and uploaded.

Scenario 1: If files are missing within the Project, contact the Members that have “Edit & Download” access level to identify and locate the missing file.
Scenario 2: If there are missing files in the View and Markup use the following steps to locate and upload those files:
  1. In Project view, choose “View & Markup”
  2. Within the View & Markup screen, Navigate to the “Pathfinder” display (in the upper right of the screen). Make note of any file names with a red “?” icon.
  1. Close the Markup view and select “Upload” in the Project view.
  2. Locate the missing file(s) and upload them to the Project.
  3. Choose “View and Markup” for the CAD assembly again and select “Update” when the Markup view appears. 


For some complex CAD files it may be necessary to re-upload the entire collection of associated files. If this is required, make sure that all the files associated with the CAD file are present and contained within the same folder.
If you have any questions or issues not addressed by this article, please work with the Support Engineer assigned to your Support Case – or if you have not yet reached out to our Technical Support team you can do so via Siemens Software Support Center: Open a Support Case.
 

KB Article ID# KB000047992_EN_US

Contents

SummaryDetails

Associated Components