Simcenter 3D Solutions Simcenter Flotherm to Simcenter 3D

2023-04-13T17:33:44.000-0400
Simcenter Nastran Simcenter 3D

Summary

How to export Simcenter Flotherm temperature results and prepare for transfer to Simcenter 3D


Details

Important note: As of Simcenter Flotherm 2210 (released October 2022),  it is now possible to easily and directly export Simcenter Flotherm 3D solid temperature field results in FLD file format for use in Simcenter 3D software for thermo-mechanical analysis workflows. Please see the details in the Simcenter Flotherm 2210 release blog article for information or see the release and download information in Support Center on Simcenter Flotherm 2210.  

This past article here below remains online as the prior workflow to serve as guided example of how to leverage Python scripting to aid generation and automation of customized results files.  It shows a method to export Simcenter Flotherm solid temperatures in an ASCII format file and then convert them to the Simcenter 3D FLD format. 

The Simcenter Flotherm ASCII FLOFEA format maps temperatures, on a part-by-part basis in the exported assembly, to 8 node hex elements. This is shown in the image below:


Simcenter Flotherm FLOFEA File

To provide a seamless import process to Simcenter 3D the results are converted to the preferred FLD format shown in the image below. 

Simcenter 3D data field (FLD) format

To obtain Simcenter Flotherm results in the FLD format the ASCII FLOFEA file is required.  The default FLOFEA export file is of a format suitable for conversion in MpCCI.  To extract results in an ASCII format the environment variable FLO_FEAASCII needs to be set to TRUE, prior to launching Simcenter Flotherm.

FLO_FEAASCII Environment Variable

After setting the environment variable the Simcenter Flotherm model can be loaded and results exported as shown in the image below.

Simcenter Flotherm FLOFEA Export

The last step of the process is to use the Python script in the download section of this Communities post.  The image below outlines the use of the script that requires the input path to the FloFEA ASCII file and optionally the output folder.  

Python Simcenter FLOFEA ASCII to Simcenter 3D FLD conversion

Please feel free to provide feedback on the usefulness of or recommendations for the script. 

Additional resource: Please watch this on-demand webinar that provides an overview of combining electronics cooling simulation data from several Simcenter CFD tools with FEA thermo-mechanical stress analysis in Simcenter 3D. It demonstrates thermal analysis examples in Simcenter Flotherm, Flotherm XT and FLOEFD software and the workflows to extract accurate 3D temperature field data and seamlessly map that to an FEA mesh for thermo-mechanical stress simulation.
Watch - Enhancing electronics thermo-mechanical analysis workflow

KB Article ID# KB000047771_EN_US

Contents

SummaryDetails

Associated Components

Other SOL101 SOL103 SOL105 SOL106 SOL107 SOL108 SOL109 SOL110 SOL111-SOL112 SOL144 SOL145 SOL146 SOL153 SOL159 SOL200 SOL401 SOL402 SOL414 SOL601-SOL701 Superelement