RLM License manager installation & license configuration for Simcenter AMESim

2022-05-11T10:25:56.000-0400

Summary

This article will help you to configure your license manager on server and client machine


Details


Summery
The window is the operating system, which is widely used in the industry due to its simplicity. Installation of AMESim is quite simple and it is working in the same way as it works on the Linux machine. This article will help you to understand “How to configure the RLM license server to access the AMESim on the Window machine? Please check the video for more details?
Pre-requisites
  1. RLM License server set up – You can download the AMESim from our support portal. There are 2 DVDs. License server setup files can be located in DVD 1.
  2. Valid license file with mac id, which is exactly similar to the mac id of your machine. Please note that, if the mac id is blank, or if you are adding the mac id by hand, then, you won’t be able to access the license. Please get the correct license file with mac id from Siemens.
Steps to install
  • You can locate the RLM license server set up at below two locations.
    • In DVD 1
    • image.png
    • In the AMESim installation folder.
    • image.png
  • Double click on “RLMLicenseServer.msi” and follow the instruction given on each interactive step. For more detail, please watch the above video.
  • If RLM installation fails, then try to install it with “RLMLicenseServer.exe”.
  • If, it fails by both methods then contact Siemens support.
  • Go to window services & Ensure that the “RLM” service is running.
  • Rename the license file to “LMS.lic” (It is not really required, but this will help to simplify the name of the license file). Copy this file at any location, where you want to be.
  • Create Environmental variable LMS_LICENSE=Path of license file/LMS.lic
  • The login name is “admin” and there is no password. We suggest to you change the password after the first login to avoid security issues. Click on status. It will show the status of the server if, it is running.
  • Now, in the web browser, type link http://localhost:5054/home.asp It should open the below page.
image.png
We can configure the Simcenter AMESim license under below three scenarios
image.png
Configuration of Simcenter AMESim License
  • Scenario 1 – Set below environmental variable.
    • On server machine – “LMS_LICENSE=5053@localhost” Or LMS_LICENSE=Path of license file\LMS.lic
  • Scenario 2 – Set below environmental variable.
    • On server machine – “LMS_LICENSE=5053@localhost” Or LMS_LICENSE=Path of license file\LMS.lic
    • On client machine – “LMS_LICENSE=5053@servername” where server name is the hostname of your license server machine.
  • Scenario 3 – Set below environmental variable.
    • On server machine – “LMS_LICENSE=5053@localhost” Or LMS_LICENSE=Path of license file\LMS.lic
    • On client machine – “LMS_LICENSE=5053@servername” where server name is the hostname of your license server machine.
.If, you are still not able to access the license by the above method, then, generate the diagnosis report and send it to our support engineer by raising the support case at this link . Please follow the below process to generate a diagnostic report.

Generate rlmdiag.txt file on server machine-
image.png
  • It will generate the rlmdiag.txt file at the path given at the output location.
image.png
  • Send the “rlmdiag.txt” file to me.
 
Generate RLMLOG.txt file on server machine-
  • Click on the Status tab at the left side. It will open the main server page. At the right side, you will see the path for the debug file log. Here, you can see the “RLMLOG.txt” file.
image.png
 System Info Snap of server machine-
  • Please also click on System Info Tab and send me the snap of the right side window.
image.png

The below articles can also help in the installation process. Please visit the below VIDEO articles.

CLICK HERE  to know about the Installation of Simcenter AMESim & RLM license configuration on Window 10 machine.
CLICK HERE   to know about How to Install Simcenter AMESim & How to configure the Simcenter AMESim RLM license on the Linux/Ubuntu Machine.
CLICK HERE   to know How to Install & Open multiple AMESim versions on the same Window machine

If you still need support or clarification, then click here to raise the case on the support portal.
 

KB Article ID# KB000046621_EN_US

Contents

SummaryDetails

Associated Components