With Simcenter STAR-CCM+ 2021.1 Siemens Digital Industries Software introduces a host of new features to help you design better products, faster and with greater confidence.
Join our Virtual Launch Event of Simcenter STAR-CCM+ 2021.1 on March 9, Live on LinkedIn to learn more
Increased insight into turbomachine performance
3D analysis of a turbomachine offers deep insight into local flow features to assess its performance. With Average Solution Visualization, you can now circumferentially average the flow solution to better visualize macroscopic features such as hub or shroud separation so that you can readily identify issues in the flow path and ensure the intended performance is achieved.
Circumferential averaging of the axial velocity field in a gas turbineAnother important data analysis tool for better engineering decisions across blade designs is the blade-to-blade view. With Section Flattening, you can now project a complex 3D blade-to-blade solution to a flattened 2D view. This helps you to understand performance, visualize flow behavior and ensures consistent comparisons between designs.
Section flattening of the complex 3D solution for better insights into blade-to-blade interactionLearn more about all the recent advancements in Simcenter STAR-CCM+ for gas turbine CFD
A faster approach to characterizing compressor performance
When characterizing compressor performance, it was often necessary to change the outlet boundary condition type when the operating point moves from choke to surge. The Corrected Mass Flow Outlet BC is a single boundary condition that can now be used to accurately predict all points along the compressor speedline, saving time and resulting in a more uniform resolution of points.
Learn more about all the recent advancements in Simcenter STAR-CCM+ for gas turbine CFD
Open simulation files without a license for increased productivity
Design engineers need to ensure consistency in their simulation set-up across operating points and design variants. In this release, you can open simulation files in read-only mode without consuming a license, giving you much greater ability to check your set-up, make comparisons and leverage your best practices across many simulations.
You can now compare Simcenter STAR-CCM+ simulations, or copy and paste setups from one file to the other without consuming a licenseFind out more about the benefits of the read-only mode for simulation files
Quickly predict performance of thousands of design variants
Tolerances can make or break manufacturing processes and need to be considered early in the design process. With Surrogate Models in Design Manager, you can predict the performance of thousands of variants either locally around your design of interest to analyze probability of failure or globally across the design space to quickly create a database of performance results that can be leveraged by your simulation team.
Learn how to leverage the power of surrogate models for faster engineering insights with confidence
Reduce setup time for electromagnetic simulations
Electromagnetic simulations require the specification of an electric circuit which can be time consuming. With the new Electric Circuit Editor, you can readily sketch sophisticated circuits with an easy-to-use and intuitive graphical interface, enhancing usability of the Circuit Model and saving time. This tool is beneficial for all applications with circuits including electric machines, circuit breakers and batteries.
Quickly set up an electric circuit with the new electric circuit editorFind out more about latest advancements on EMAG simulations in Simcenter STAR-CCM+
Design higher power density electric machines
In this release, we continue to expand the application coverage for electric machines with the introduction of a new vector method to specify the current direction when using the Finite Element Excitation Coil Model. This approach does not require the presence of any boundary, greatly improving the usability of the Excitation Coil Model and enabling the simulation of closed coils such as those found in axial flux machines.
The newly implemented vector method in action: a graphical method to specify the current by simply placing a point and an arrow in your SceneFind out more about latest advancements on EMAG simulations in Simcenter STAR-CCM+