Simcenter Testlab Displays: Locked and Scrolling Data

2020-02-01T18:25:10.000-0500

Summary


Details

User-added image

Want to scroll through some data while comparing it to a reference curve?  The new “Lock” display feature of Simcenter Testlab 2019.1 is just for you!


Here is how it works:

1. First put select some data for interactive viewing in a display:
 
User-added image
 
2. The click on the double arrow icon in the upper right above the display to open the scrolling mode. Select a function to use for scrolling.  For example, “Section Value” scrolls by order number.
 
User-added image
 
3. Click on the Single Arrow button to increment each function in the display by one at a time.
 
User-added image
4. Click on the Double Arrow button to scroll through all data in display as a group.
User-added image
 
5. To lock, or freeze, one of the curves permanently in the display, right click on it in the legend and choose “Lock”.
 
User-added image
 
6. Even while using the scrolling button, the Locked curve will stay in place in the display.
User-added image

Enjoy the locking and scrolling features of Simcenter Testlab when viewing data.

Questions?  Email peter.schaldenbrand@siemens.com or contact Siemens Support Center
 

Simcenter Testlab Display tips:

KB Article ID# KB000044427_EN_US

Contents

SummaryDetails

Associated Components