Direct YouTube link: https://youtu.be/pe80EeDmwqo
There are two types of forces that can be used in Transfer Path Analysis:
This article explains the differences between these types of forces, how they are calculated, and in what circumstances they are used.
The article has the following sections:
1. Background and Motivation
2. Contact Forces
2.1 Mount Stiffness Based Contact Force Estimation
2.2 Matrix Inversion Contact Force Estimation
3. Blocked Forces
3.1 Rigid Boundary Blocked Force Estimation
3.2 Free Boundary Blocked Force Estimation
3.3 In-situ Blocked Force Estimation
4. Analytical Example
4.1 Contact Forces
4.2 Blocked Forces
4.3 Using Blocked Forces with New Receivers
5. Blocked Force Application Case
6. Conclusion
1. Background and Motivation
Contact and blocked forces are often used in Transfer Path Analysis (TPA). Transfer Path Analysis is a technique used to understand the important dynamic paths in a source-receiver system that generates vibration or sound.
In a Transfer Path Analysis (Figure 1):
Figure 1: Operational forces (orange, Fo) are multiplied by structural sensitivities (green) to determine vibration at a receiver location. In this case, the operational acceleration (Ao) at the receiver location is of interest.
The operating dynamic force (Fo) is multiplied by the transfer function (H) for each load path. By evaluating the results of the multiplication, the largest contributor to sound or vibration can be determined.
To perform a Transfer Path Analysis, the FRFs and operational forces can originate from either simulation or test data:
Contact and blocked force estimation from test data are explained in the next section. For the remainder of the article, operational forces and accelerations will not have a subscript o to indicate operational conditions, and FRFs will be referred to with a H.
2. Contact Forces
Contact forces are useful in troubleshooting noise and vibration problems. They are the forces that are active on the receiver system.
Typical test methods for estimating contact forces include mount stiffness based estimation and FRF matrix inversion:
2.1 Mount Stiffness Based Contact Force Estimation
Using operational accelerations and dynamic stiffness curves, a mount-based estimation method can be used to determine the forces (F) acting within a source-receiver system.
The method is based on Hooke’s law, where force equals stiffness times displacement (F=kx). In the mount method, the mount stiffness (K) is multiplied by the displacement (x) across the mount. Typically, acceleration (A) is measured on either side of the mount, double integrated, then subtracted, to get displacement.
A source-receiver system can have multiple inputs and multiple outputs. A simplified diagram of such a system is illustrated in Figure 2.
Figure 2: Contact forces estimated from mount stiffness use the stiffness curve (K) and relative displacement across the mount.
In Figure 2, there are inputs and outputs on the source and receiver systems indicated by numbered dots. Even though a single dot is shown, each dot can represent multiple input or multiple output locations of each system:
In the equation, the following frequency-based functions are used:
It should be noted that Figure 2 is a simplified representation of a source-receiver system. A real-life system has multiple attachment locations between the source and receiver. For example, a motor (source) could be attached with four mounts to a vehicle body (receiver) as shown in Figure 3.
Figure 3: Application example of source-receiver system with complex system dynamics and multiple interface locations.
Another method for estimating forces from test measurements is called the matrix inversion method.
Matrix Inversion Contact Force Estimation
In matrix inversion, the force estimation is based on multiplying an inverted matrix of local driving point FRFs (in the form of A/F) by the operational accelerations at the same locations as shown in Figure 4.
Figure 4: Contact forces estimated from FRF matrix inversion on the input locations of the receiver system.
The basic equation for the force estimation is (A/F)-1 * A. The operational acceleration at the input location on the receiver is measured and multiplied by the inverse of the measured transfer functions (H-1, with units F/A) at the same input locations.
In Figure 4, the following frequency based functions are used:
Contact forces are often used in troubleshooting source-receiver systems. By calculating the multiple contact forces applied to the receiver system, the locations that cause the largest receiver responses can be identified.
Because the contact forces are determined at the input to the receiver, they already contain the dynamics of the source. They should only be applied on the receiver system alone to predict vibration or sound. Contact forces are calculated for a specific receiver and cannot be used when a different receiver is introduced into the system
Instead of calculating contact forces, blocked forces could be estimated from the same source-receiver system.
3. Blocked Forces
Blocked forces are characteristics of just the source system by itself. To calculate a blocked force, the source system must be isolated (by either a completely rigid or completely free boundary condition). If a source system cannot be isolated, the influence of the receiver can be removed through a FRF based inversion process called in-situ force estimation.
3.1 Rigid Boundary Blocked Force Estimation
To calculate the blocked forces of a source, the outputs must be clamped or blocked as shown in Figure 5. This is done by connecting the source to an infinitely rigid boundary.
Figure 5: If the source output locations are connected to an infinitely rigid boundary, the forces at outputs are blocked forces.
In Figure 5, the following notation is used:
In practice, measuring operating forces from a source in a rigid boundary condition can be challenging. An infinitely rigid boundary condition is hard to build. An example attempt is shown in Figure 6.
Figure 6: Attempt to create a rigid fixture for performing force calculations on a tire.
Even if built rigidly, real world objects are never infinitely rigid, especially from a dynamic point of view.
Instead of trying to create a rigid connection, blocked forces can also be calculated from a free boundary condition.
3.2 Free Boundary Blocked Force Estimation
Mathematically, it can be proven that blocked forces can also be derived from measurements at the output locations, if the source is suspended in free-free conditions (Figure 7).
Figure 7: Blocked forces can be calculated at the output of the source under free boundary conditions.
In Figure 7, the following notation is used:
This boundary is sometimes referred to as free acceleration or free velocity conditions.
In practice, it can be difficult to achieve a free-free boundary condition. Imagine trying to run a source while it is suspended in mid-air!
3.3 In-Situ Blocked Force Estimation
Neither the infinitely rigid nor the free boundary condition is easy to achieve in practice. Instead the blocked forces can also be derived from in-situ measurements where both the source and receiver are present.
Transfer functions between the source output locations and the receiver indicators are used to “back out” the effects of the receiver on the source output forces (Figure 8).
Figure 8: Blocked forces can be calculated from in-situ measurements (for example, an engine on a fixture). To do so, FRF inversion combined with measured operational data is used to calculate blocked forces at the output of the source.
In Figure 8, the following notation is used:
The methodology for calculating blocked forces in-situ is similar to the matrix inversion method used for contact forces. For soft mount connections between the source and receiver, forces are calculated at the output of the source (for blocked forces) rather than the input of the receiver (for contact forces via matrix method). Another important difference is that when calculating contact forces, the FRFs are measured/calculated without the source present. With blocked forces, both the source and receiver are present.
One challenge in the blocked forces measurement is the difficulty measuring transfer functions in assembled conditions due to the limited accessibility of many mounting points.
For more information on obtaining blocked forces from different assemblies, see the article: Obtaining Invariant Loads: Practical Examples.
Next, examples of how and when contact forces should be used versus blocked forces will be illustrated through an empirical example.
4. Analytical Example
Consider the source-receiver system shown in Figure 9. It consists of four different masses (m1, m2, m3, and m4) connected by springs (k) and dampers (c). Part of the system is designated the source (S) and part is the receiver (R).
Figure 9: A dynamic mass-spring-damper system with a source (S) and receiver (R). The force input (Finput) at the source results in a velocity of the receiver (R).
In this system:
A 1000 Newton dynamic force (Finput) is applied on Mass1 of the source system (S) from 0 to 1000 Hertz. It results in a velocity (v4) of System R as shown in Figure 10.
Figure 10: Left – A 1000 Newton input force is applied to the source system (S) from 0 to 1000 Hertz. Right – The velocity output (v4) is plotted of the receiver (R) system.
This velocity of the receiver (v4) due to Finput will be used as a reference. Contact and blocked forces will be applied at the interface of the source (S) and receiver (R) systems and compared to the reference in the next examples. Initially, as shown in Figure 11, the contact force will be calculated and used.
4.1 Contact Forces
A contact force (Fc) at the interface of m3 (system R) can be calculated from the original system due to Finput. This is often what is done in Transfer Path Analysis applications. The Finput is rarely known in real life. For example, it is easier to take measurements at the mount attachment locations of a motor or engine than to measure inside of it.
After calculating the contact forces, they are applied to the source-receiver (SR) system and to just the receiver (R) as shown in Figure 11. While Finput is used to calculate v4 on the left side of Figure 11, it is not used in the middle and right systems. Only the contact force (Fc) is applied.
Figure 11: When contact forces (left, blue) are applied to the combined system SR, then the output velocity (v4) does not match the reference velocity (middle, red). When contact forces are applied to system R, the output velocity (v4) matches the reference velocity (right, green).
The following can be observed about the velocity outputs of the systems with only the contact force applied:
The velocity output versus frequency is shown in Figure 12.
Figure 12: The velocity (v4) of the receiver system (R) is shown in blue. Applying contact forces to just system (R) results in a match between the reference velocity and output velocity (green). Applying the contact force to the combined source-receiver system does not match (red).
To get the correct output, the contact forces were applied to the receiver system (R) alone.
How would the force have to be adjusted to get v4 to match when it is applied to both systems S and R? This is the blocked force which is discussed next.
4.2 Blocked Forces
If the source system (S) is hooked up to an infinitely stiff and massive object, blocked forces can be calculated as shown in Figure 13.
Figure 13: Blocked forces from source system (S) can be calculated by attaching an infinitely stiff and massive object.
For the blocked force calculation, the source-receiver definition will be changed slightly compared to the contact force calculation. Instead of calculating the force input on the receiver, the force output of the source will be calculated.
The blocked forces can then be applied to the both source-receiver system (SR) and just the receiver system (R) as shown in Figure 14.
Figure 14: When blocked forces (left) are applied to the combined system SR, then the output velocity (v4) matches the reference velocity (middle, green). When blocked forces are applied to system R, the output velocity (v4) does not match the reference velocity (right, red).
Applying the blocked forces from the source system (S), the output velocity (v4) of the combined source-receiver (SR) system matches the reference velocity exactly, as shown in Figure 15.
Figure 15: Using blocked forces, the output velocity (green) of the combined source-receiver system (SR) matches the reference velocity due to Finput (blue). When blocked forces are applied to system R alone, the output velocity (red) does not match the reference (blue).
Applying the block force to only system R does not yield the correct results (red line in Figure 15 above).
Contact forces yield the correct results when applied just to the receiver system alone. Blocked forces yield the correct results when applied to the combined source-receiver system. The advantage of blocked forces come about when introducing a new receiver system, and then trying to predict the new system output. This is discussed in the next section.
4.3 Using Blocked Forces with New Receivers
A new receiver system (T) is introduced as shown in Figure 16. It has new masses: Mass 5 and Mass 6.
Figure 16: The new receiver system (T) has and output velocity (v6) spectrum.
The source system (S) is the same as before. The same Finput is applied, but a new velocity (v6) is produced on the receiver (T).
The new receiver system (T) is composed of:
The previously calculated block (from system S attached to infinitely rigid mass) and contact forces (from systems SR) can be applied to the new receiver system as shown in Figure 17. The velocity output created by these forces can be compared to the reference velocity (v6).
Figure 17: When applying blocked forces (Fb) derived from the source system (S) to the combined source-receiver system (ST), the output velocity matches the reference velocity (left, blue). Applying the contact forces (Fc) to the new receiver system (T) does not match the reference (right, red).
Using the blocked forces from system (S), the output velocity (v6) of the combined source-receiver system (ST) matches the reference velocity. However, when using the contact forces of original source-receiver system SR, the output velocity (v6) is not correct. This is shown in Figure 18.
Figure 18: Using blocked forces, the output velocity (green) of the combined source-receiver system (ST) matches the reference velocity (v6) due to Finput (blue). When contact forces are applied to the new receiver system (T) alone, the output velocity (red) does not match the reference (blue).
In this situation, blocked forces have an advantage over contact forces. The blocked forces can be used to predict the output of a new system, where the contact forces cannot.
In this empirical example, single attachment locations were used between masses. In real world applications, multiple attachments are often required. The techniques work for multiple attachment locations also.
An example application case is discussed below to demonstrate the use/advantage of blocked forces.
5. Blocked Force Application Case
One use for blocked force is to determine the source forces “upfront” from test rig measurements during the development process.
Often, a source (for example, a motor, pump, or engine) is available in the test rig before its receiver application (for example, a vehicle, train, or ship) is available.
If a dynamic CAE simulation model of the application is available, the test fixture forces can be combined with the dynamic FRFs to predict the vibration or sound of the assembly before it is completely built. This allows problems to be identified and resolved before the source is ever installed in real life.
To illustrate this situation, a small test rig and application structure was created as shown in Figure 19. The same source was used in both the test rig and application fixture.
Figure 19: Left – Test rig fixture with source (black/white hash lines) mounted on top. Right – Application fixture with source (black/white hash lines).
Photos of the actual fixtures are shown in Figure 20. An electro-dynamic shaker was attached to the source to create a force.
Figure 20: Left – Photo of source attached to test fixture. Right – Photo of source with shaker attached on application fixture.
The vibration on a key area on the application fixture was predicted using contact and blocked forces derived from measurements on the test fixture. Using the blocked forces from the test rig, the predicted acceleration matched the measured closely (Figure 21) for the application fixture.
Figure 21: Using blocked forces from a test bench, the calculated vibration response (green) predicts the measured vibration response (black) closely on the application fixture.
When applying the contact forces from the test fixture to the application rig, the resulting prediction is not close, as shown in Figure 22. This is because the contact forces were calculated specifically for the test rig fixture, not the application fixture.
Figure 22: Measured acceleration response (black) on application fixture versus predicted acceleration response (blue) from test rig derived contact forces applied to application fixture.
Blocked forces have an advantage over contact forces for predicting the dynamic behavior of new receivers when they are introduced into an existing source-receiver system. They can be used to predict the new receiver response.
The contact forces from an existing source-receiver system cannot be transferred to a new receiver. They will not give accurate results because the forces are dependent on the original receiver system. The contact forces are not properties of the source system alone.
The blocked forces are invariant with respect to the receiver. The blocked forces are properties strictly of the source system. Blocked forces must always be applied to a combined source-receiver system for accurate predictions at receiver locations. When combined systems are not available, they can be predicted using tools like FRF Based Substructuring.
Conclusion
Blocked forces enable sources to be evaluated in different applications without having to test each situation. This allows force sources to be characterized on test benches and confidently integrated in new, untested applications.
Using the blocked force approach, libraries of source and receiver components can be created and combined to build accurate virtual TPA models. This allows original equipment manufacturers to evaluate dynamic assembly options without having to build costly prototypes.
Questions? Email peter.schaldenbrand@siemens.com or download the Component Based Transfer Path Analysis White Paper.
Related Links: