Simcenter STAR-CCM+ Simcenter STAR-CCM+ Viewer Download

2023-11-28T13:56:29.000-0500
Simcenter STAR-CCM+ Simcenter STAR-CCM+ Virtual Reality Teamcenter Share Simcenter Cloud HPC Simcenter STAR-CCM+ Viewer Simcenter STAR-CCM+ Application Specific Solutions

Summary


Details

The Simcenter STAR-CCM+ Viewer is a lightweight, license-free standalone scene and plot viewer for Simcenter STAR-CCM+.

User-added image

You can use it to examine a scene or plot as you would in Simcenter STAR-CCM+ when the display contents are exported to a three-dimensional .sce graphics file. As an alternative to running the full Simcenter STAR-CCM+ client, this file format is strictly for interactive viewing. You cannot make scene or plot modifications as you would in Simcenter STAR-CCM+, such as adding parts to be displayed, changing the colouring or using a different scalar.

You can download the latest version of the viewer here

KB000043434_EN_US

Contents

SummaryDetails

Associated Components

Design Manager Electronics Cooling In-Cylinder (STAR-ICE) Job Manager Simcenter STAR-CCM+