Direct YouTube link: https://youtu.be/es1tbX_kOHU
Want to compare data from different runs quickly in Simcenter Testlab (previously called LMS Test.Lab)?
Want to calculate the average, standard deviation, or envelope of these runs?
It is all possible using the Run Data Averaging and Comparison Organizer in Simcenter Testlab!
The Run Data Averaging and Comparison Organizer (hereby referred to as Compare Runs) add-in in Simcenter Testlab is an excellent way to average and compare runs both online in the Measure workbook and off-line in the Compare Runs workbook.
Getting Started
Begin by going to Tools / Add-ins
Figure 1: Go to Tools/Add-ins
Select Run Data Averaging & Comparison Organizer . If using Simcenter Testlab token licensing, this uses 16 tokens.
Figure 2: The "Add-ins" window.
The add-in includes both online and offline functionality.
In either case, five averaging functions are added.
Figure 3: Definitions of the five functions.
This article is composed of two sections. The first section will cover the online functionality of Compare Runs. The second section will cover the offline functionality of Compare Runs.
SECTION 1: ONLINE RUN COMPARISON
After activating the Compare Runs add-in five averaging functions are added to the Measure workbook of Simcenter Testlab Signature.
Figure 4: The Measure workbook before and after the Compare Runs add-in is activated.
Compare Runs will also add information into the Data Explorer. Any 2D function that can be averaged will appear under the Compare Runs folder.
Figure 5: Explore the Compare Runs folder in Data Explorer to see what functions you can compare across runs.
Online Run Comparison Example
For this example, three runs were acquired.
Each run consisted of a single tone.
Each run was acquired using a stationary acquisition consisting of 13 averages over 3 seconds.
1. To begin, drop data into the display from the Compare Runs folder. In this case, a stationary autopower acquisition was done. So, there is an AutoPower Mic selection available. Drag from the LEFT pane into the display.
Figure 6: Any 2D functions will be available under the Compare Runs folder.
2. Next, select which averaging functions to display in the Measure workbook. For this example, the average function is displayed. Users can display any combination of the Compare Runs functions by toggling on or off the function buttons on the upper right of the plot display area.
Figure 7: Five functions are available with the Compare Runs add-ins.
3. Under the More button, there are three online averaging display options. For this example, All runs is selected.
Figure 8: Select which runs to display under the More button.
A. No run display will not display any of the runs as they populate. The averaging functions selected will
B. Last run only will display only the most recently acquired run in addition to the averaging functions selected.
C. All runs will display all acquired runs in addition to the averaging functions selected.
4. The result after Run 1 (a tone at 1000Hz) is shown below. Run 1 is displayed in red. The average of all runs is displayed in black. In this case, the two curves are the same, so they overlap completely.
Figure 9: The first run and average of all runs are displayed. After only one run these values are the same.
5. The result after Run 2 (a tone at 1500Hz) is shown below. Run 1 remains displayed in red because the online averaging run display mode is set to All runs . As each run is acquired, the run will populate and remain as the additional runs are acquired. Run 2 is displayed in purple. The average of the two runs is displayed in black.
Figure 10: The display mode is set to All runs ; the runs populate over one another and remain in the display.
6. The third and final run is then acquired (a tone at 2000 Hz). Run 3 is displayed in green. The original two runs remain in the display and the average function updates to include the third run.
Figure 11: The runs continue to populate in the display and the average function updates appropriately.
7. When finished acquiring data, go to the Compare Runs workbook. Here is where you will save the averaging functions across your runs. 1) Select which averaging functions you would like to be save by toggling the function buttons. 2) Press Save
Figure 12: The Compare Runs workbook.
8. Users can either save just the selected functions or save all the functions. Name the folder then click OK to save.
Figure 13: Save the functions.
9. The functions will be saved to the folder in the Navigator workbook. In this case, just the average function was saved. Browse to the data block and display it.
Figure 14: Just the average function was saved.
Figure 15: All functions are saved.
Online run comparison is a great tool to instantly check your run data average!
SECTION 2: OFFLINE RUN COMPARISON
It is possible to compare runs offline. These runs can come from any project or section.
In the offline mode, analysis begins in the Compare Runs tab.
Figure 16: Compare Runs tab.
The Compare Runs workbook has four main panes.
Figure 17: Compare Runs workbook.
Data Source Selection
It is possible to import runs via the input basket or from the active project. Use the radio buttons to determine what the data source is.
Figure 18: Select to import from the Input Basket or Active project.
Once the data is imported, the Run Selection and Function Selection areas will populate.
Figure 19: The Run Selection and Function Selection areas are populated once the data is imported.
Run Selection
In the Run Selection area, there are two columns of checkboxes on the far right (see Figure 20).
It is important to note that a function may be included in the average even if it is not displayed. It is wise to inspect which of these boxes are checked before saving your averaged run data.
Figure 20: The Display and Averaging columns determine which runs are displayed and which runs are used to calculate the averaging functions.
Function Selection
There are three different ways to display the functions: Point by Point, Function by Function, or User Defined Layout. To choose a display type, click either P,F, OR U in the lower right corner of the Function Selection area.
Figure 21: P: Point by Point. F: Function by Function. U: User Defined Layout.
NOTE:
In the user defined layout mode, there is one extra step to be aware of.
If a multi-plot display is opened, the number of plots in the display will correspond to the number of buttons that become sensitive to the left of the P, F, and U.
Figure 26: The user defined mode. Here the third graph is selected. The dotted line around the third plot indicates it is the active plot.
To select which functions to display, toggle the boxes in the upper right corner of the Function Selection area. The functions are defined at the top of the article in Figure 3.
Figure 27: The averaging functions are in the top right corner.
To control how many points/ functions are displayed, click on Options in the Function Selection area.
Adjust the numbers for Functions per display and Points per display .
Figure 28: The Options window in Compare Runs.
Saving Average Run Data
Finally, save your data. Choose where to save your data, which functions to save, and what to call your new folder.
Figure 29: The Save window in Compare Runs.
Enjoy the power of the Compare Runs workbook!
Questions? Email scott.beebe@siemens.com, contact Siemens Support Center, or post a reply!
Simcenter Testlab Acquisition Tips
Simcenter Testlab Processing Tips