Simcenter Testing Solutions What is a SN-Curve?

2019-08-29T16:35:56.000-0400
Simcenter Testlab

Summary


Details


Direct YouTube link: https://youtu.be/15BVllILXFo


*** Free On-Demand Webinar - Fundamentals of Durability Engineering ***

 

What is a SN-Curve?

User-added imageA SN-Curve (sometimes written S-N Curve) is a plot of the magnitude of an alternating stress versus the number of cycles to failure for a given material. Typically both the stress and number of cycles are displayed on logarithmic scales.

Given a load time history and a SN-Curve, one can use Miner's Rule to determine the accumulated damage or fatigue life of a mechanical part.

History

SN-Curves were developed by the German scientist August Wöhler (Figure 1) during the resulting investigation of an 1842 train crash in Versailles, France. In this crash, the axle of the train locomotive failed under the repeated “low level” cyclic stress of everyday usage on the railroad.

AugustWohler.png
Figure 1: August Wöhler (1819 to 1914) developed SN-Curves to understand railcar axle failures

While investigating, Wöhler discovered that cracks formed and slowly grew on an axle surface. The cracks, after reaching a critical size, would suddenly propagate and the axle would fail. The level of these loads was less than the ultimate strength and/or yield strength of the material used to manufacture the axle.

Wöhler developed an apparatus to apply repeated loads to railroad axles and chart the relationship between load level and number of repeated cycles to failure. “Wöhler Curves” plot the relationship of alternating/cyclic stress levels against the number of cycles to failure.

Designing an axle to withstand the initial static loads associated with holding up a locomotive was well understood. It was fairly obvious if an axle could carry the weight of a train if it did not collapse immediately. The concept of low level cyclic stresses, repeated over a long time, was relatively new and not well understood. For many observers at the time, it seemed unpredictable when an axle might suddenly fail. It was not until Wöhler developed his SN-Curves that cyclic stress became better understood, and fatigue life could be predicted in a more consistent manner.

How is a SN-Curve created for a given material?

Today, these curves are often developed by using a metal coupon testing machine (Figure 2). A small metal coupon is placed into the machine and subjected to a cyclic (or alternating) stress time history until a crack or failure occurs in the metal coupon.

SN_Development.png

Figure 2: Coupon testing is used to create SN-Curves for materials

Several coupons must be tested at different stress levels to develop a SN-Curve. Figure 3 illustrates a typical SN-Curve derived from testing metal coupons.

SN_Curve.png
Figure 3: SN-Curve for a material: Higher amplitude stress cycles resulting in lower number of cycles to failure

A SN-Curve functions as a “lookup table” between alternating stress level and the number of cycles to failure (Figure 4). Most SN-Curves generally slope downward from the upper left to the lower right. This indicates that high level amplitude cycles have fewer number of cycles to failure compared to lower level amplitude cycles.

SN_Curve_with_Lookup.png
Figure 4: SN-Curve relating Alternating Stress Level to corresponding Number of Cycles to Failure via dashed dark blue line

In a fatigue test like this, the frequency at which the cycles are applied is not considered to be a factor in the number of cycles to failure. It is strictly the number of cycles, and not the rate at which the cycles are applied, that affect the SN-Curve results.

In real life, the frequency of the cycles can be a factor, especially if the loading frequency coincides with a natural frequency or resonance of the object which amplifies the magnitude of the cycles.

Plastic, Elastic and Infinite Regions

A SN-Curve can contain several different areas: a plastic region, an elastic region and an infinite life region as shown in Figure 5.

SN_Curve_Key_Points.png
Figure 5: Ultimate Strength, Yield Strength and Endurance Limit on SN-Curve

There are three key values that separate the plastic, elastic and infinite life regions (Figure 5):

  • Ultimate Strength: Stress level required to fail with one cycle
  • Yield Strength: Dividing line between elastic and plastic region
  • Endurance Limit: If all cycles are below this stress level amplitude, no failures occur

Several of the values on the SN-Curve can be found by doing a static stress-strain test on a material coupon (see Figure 6).

StaticStressStrain_vs_SNCurve.png
Figure 6: Ultimate Strength and Yield strength can be determined from static stress-strain tests

For example, the Ultimate Strength stress is the value that causes a failure for one cycle. The Yield Strength stress level divides the plastic and elastic region.

Infinite Life

Some materials, like steel, exhibit an infinite life region (Figure 7). In this region, if the stress levels are below a certain level, an infinite number of cycles can be applied without causing a failure (of course, no test has been performed for an infinite number of cycles in real life, but a million+ cycles is typical).

SN_Curve_InfiniteLife.png
Figure 7: Infinite life region of SN-Curve

Critical components (ie, engine crankshafts and rods) are usually designed for infinite life because cycles are speed dependent and accumulate quickly. All the cyclic stress levels that the part is subjected to must be below the endurance limit to have infinite life.

Infinite life is not in effect under certain conditions:

  • Infinite life is only based on number of stress cycles, it assumes corrosion and other factors are not present.
  • If any of the cyclic stress levels are higher and in the plastic or elastic region, then the endurance limit is no longer in effect.

Different metals have different endurance limits. Some typical endurance limits are show in Table 1.

EnduranceLimitTable.png
Table 1: Typical Endurance limits of specific metals

Many non-ferrous metals and alloys, such as aluminum, magnesium, and copper alloys, do not exhibit well-defined endurance limits (Figure 8).

EnduranceLimit_Steel_vs_Aluminum.png
Figure 8: Endurance limit of aluminum (red) is not as well defined as steel (green)

Where steel has a definite change in slope at the endurance limit, aluminum and other metals do not always have a distinct change.

To determine if a part or object is operating in the infinite life region, the Goodman-Haigh diagram is often used.  In addition to the cycle amplitude, mean stress is also accounted for in the Goodman-Haigh approach.

Elastic Region

In the elastic region (Figure 9), the relationship between stress and strain remains linear. When a cycle is applied and removed, the material returns to its original shape and/or length. This region is also referred to as the “High Cycle Fatigue” region, because a high number of stress cycles, at a low amplitude, can cause the part to fail.

SN_Curve_Elastic.png
Figure 9: Elastic life region of SN-Curve

Typical factors that influence the performance of a material in the elastic region are residual stresses and geometric considerations. For example, a severe geometry change in the material may be more likely to have a crack initiate than a smooth geometry change.

Plastic Region

In the plastic region (Figure 10), the material experiences high stress levels, causing the shape and/or geometry to change due to the repeated application of stress cycles. This region is also referred to as the “Low Cycle Fatigue” region of the SN-Curve, where a low number of stress cycles, with a high amplitude, result in failure.

SN_Curve_Plastic.png
Figure 10: Plastic life region of SN-Curve

Material plasticity and geometry are big influences on the number of cycles to failure in the plastic region.

Calculating fatigue life or damage in the plastic region of a material with a SN-Curve is probably best avoided. If cyclic stress levels are in the plastic region, a strain life approach would typically be recommended instead, which includes an E-N (Strain vs Number of cycles) as part of the analysis. Strain life also takes into account the order or sequence in which loads are applied.

SN-Curve Libraries

Tests for materials can be expensive to run. Ideally, the tests should be repeated many times and at many different stress levels. With enough experiments, the SN-Curve would consist of a series of confidence intervals around the main curve as shown in Figure 11.

SN_Curve_statistics.png
Figure 11: SN-Curve consists of many individual tests and is actually a curve fit to a distribution of data (black dots)

Some materials have well known curves because they are very commonly used. Some materials do not. When a new alloy is developed, the SN-Curve may be completely unknown and testing will be required to determine the curve. Conventionally, five different stress levels with three repeats at each level is considered the minimum to determine a SN-Curve.

The book “FKM Analytical Strength Assessment” contains many material SN-curves. It is published by the VDMA (Verband Deutscher Maschinen- und Anlagenbau e.V.), a German engineering association of engineering companies, which includes Siemens.

Logarithmic Nature of SN-Curve: Double amplitude vs Double cycles example

Consider the following hypothetical time histories to be evaluated for damage:

  1. Alternating Stress of 300 MPa for 1000 cycles
  2. Alternating Stress of 300 MPa for 2000 cycles
  3. Alternating Stress of 600 MPa for 1000 cycles

First consider time history #1 and time history #2 shown in Figure 12. These time histories have:

  • The same amplitude cycles
  • Different number of cycles (one is double the other)

TimeHistory1vsTimeHistory2.png

Figure 12: Time history #1 vs Time history #2

Using Miner's Rule, one sees that the cumulative damage of time history #2 is double compared to time history #1 (see Figure 13).

DoubleDamage.png
Figure 13: Cumulative cycle count and cumulative damage of Time history #1 vs Time history #2

Next compare the damage potential in load time history #1 vs time history #3 shown in Figure 14. These time histories have:

  • Different amplitude cycles (time history #3 is double the amplitude of time history #1)
  • Same number of cycles

TimeHistory1vsTimeHistory3.png

Figure 14: Time history #1 vs Time history #3

Using Miner’s Rule to analyze the load time history with a SN-Curve, one sees that the cumulative damage of time history #3 is 20 times compared to time history #1 (Figure 15), even though the amplitude of the cycles are only double in time history #3 compared to time history #1.

20TimesDamage.png

Figure 15: Cumulative cycle count and cumulative damage of Time history #1 vs Time history #3

Why does doubling the stress level result in twenty times the damage? This is because the SN-Curve is actually a log vs log graph, which is easy to forget when viewing what appears to be straight lines in the log-log respresentation of the SN-Curve (Figure 16).

Log_vs_Linear_SNCurve.png

Figure 16: SN-Curves plotted in Linear vs. Linear and Log vs. Log

The relationship between stress level and number of cycles to failure is not linear, which has very important implications for fatigue life.

SN-Curve Slope: K-factor

The slope of the log-log SN-Curve is defined by “k-factor”. This "k-factor" governs the relationship between the stress level and the number of cycles to failure.

The "k-factor" was developed by Wöhler to easily relate the load (ie, stress) to the life (number of cycles to failure). Figure 17 shows how the Wöhler curve relates load to life via the k-factor in the elastic region of a SN-Curve.

kfactor.png
Figure 17: Slope of SN-Curve is expressed by the k-factor

Because of this log vs log relationship, it means that a small change in load amplitude can have a very large change in the fatigue life or damage. In Table 2 below, with k-factor of 5, a 15% change in load results in a factor of 2 change in damage/fatigue life.

kfactor_table.png
Table 2: k-factor versus stress level and fatigue life

The logarithmic relationship between alternating stress level and the number of cycles to failure is an important consideration in accelerating fatigue testing. As the k-factor gets larger, small increases in load (ie, stress) create larger and larger changes in life. This can be used to accelerate a durability test. By increasing the load a small amount, so that the failure mode is not changed, one can still get large reductions in test time.

As a general rule of thumb, one can associate the following k-factors with the following:

  • k-factor of 7: Aluminum
  • k-factor of 5: Steel
  • k-factor of 3: Welds

SN-Curve adjustments due to Mean Stress

When using SN-Curves, there can be extenuating circumstances where the SN-Curve must be adjusted to reflect certain situations.

Take the stress time history in Figure 18. The average or mean stress of the cycles is zero.

MeanStressZero.png

Figure 18: Cyclic stress cycles with mean stress of zero

Why track the mean stress? In real world loading situations, there could be a mean stress other than zero acting on the part. For example, the suspension system of a car has to carry the static weight (or load) of the car. As the car drives on the road, cyclic stresses/loads are applied by bumps in the road while the car weight is applying a mean stress (which is not zero).

There are two different types of mean stress that a part may encounter: tension and compression.

In the case of tension (Figure 19), there is a positive mean stress. In a metal coupon test, a static tensile mean stress creates a load that tries to pull the coupon apart.

MeanStressTesnsion.png

Figure 19: Cyclic stress cycles with positive mean stress greater than zero (tension)

This additional tension reduces the number of cycles to failure. The part would fail sooner than the SN-Curve with mean stress of zero would predict.

The static mean stress could also be pushing the part together, creating compression (Figure 20). This compression would extend the life of the part, making it last longer than the zero mean stress SN-Curve would predict.

MeanStressCompression.png

Figure 20: Cyclic stress cycles with negative mean stress greater than zero (compression)

Mean stress effectively shifts the SN-Curve up or down (Figure 21). A tensile mean stress in effect shifts the SN-Curve downward so it takes fewer number of cycles to fail. A compressive mean stress shifts the SN-Curve upward so the number of cycles to failure is higher.

SN_Curve_Mean_Stress.png

Figure 21: SN-Curve adjustments due to mean stress

Typically, SN-Curves are developed for a specific “Stress Ratio” as shown in Figure 22. The “stress ratio” called R is the lower value of the stress divided by upper value of the stress in cyclic stress time history. It is a convenient way to designate the conditions for a SN-Curve test. For example, in the aerospace industry, many components are tested with a stress ratio of 0.1, which ensures a net tension on the component.

StressRatio.png

Figure 22: Diagram of stress ratios

For fully-reversed loading conditions with mean stress of 0, R is equal to -1. For static loading, R is equal to 1. For a case where the mean stress is tensile and equal to the stress amplitude, R is equal to 0.

For more information, read the article on Mean Stress and Stress Ratios.

SN-Curve Adjustments due to Loading

How the load is applied to the structure makes a difference in the number of cycles to failure. The load can be applied in several ways: torsional, bending, axially, etc as shown in Figure 23.

SN_Curve_Loading_Adjustments.png

Figure 23: Different types of loads/stresses

The load scaling correction factors (Cf) are different and depend on the material. The correction factors are used to scale the stress up or down based on the type of load being applied. In the case of Bending vs Torsion for the material in Figure 23, the adjustment is 40%.

Other SN-Curve Adjustments

There are many other reasons why a SN-Curve may need to be adjusted. Other SN-Curve adjustments include part size, surface finishes, notches in the geometry, etc.

Questions? Email peter.schaldenbrand@siemens.com

More Fatigue and Durability links:

KB Article ID# KB000043081_EN_US

Contents

SummaryDetails

Associated Components

Simcenter Testlab Digital Image Correlation Testlab Environmental Testlab Acoustics Testlab Data Management Testlab Desktop Testlab Durability Testlab General Acquisition Testlab General Processing & Reporting Testlab Rotating Machinery & Engine Testlab Sound Designer Testlab Structural Dynamics Testlab Turbine