Simcenter Testing Solutions Simcenter Testlab Recording Workbook Download

2020-08-21T12:36:43.000-0400
Simcenter Testlab

Summary


Details

dsp_icon.png

The Simcenter Testlab Recording Workbook application has the following capabilities::

  • Channel Setup: Can configure transducer information for the channels on Simcenter SCADAS hardware.
  • Display: Has a viewer for a wide variety of file formats (RPC, LDSF, Universal, etc) including those acquired by SCADAS hardware.
  • Data Conversion: Write time recordings measured with the Simcenter SCADAS Recorder, SCADAS RS, or Simcenter SCADAS XS to many formats in one step. Recorder Data Conversion Tool Instructions.

With Simcenter Testlab Revision 2021.1 and lower, the Simcenter Testlab Recording workbook was called the Recorder Data Conversion tool.. The name was changed to Simcenter Testlab Recording Workbook to reflect new capabilities that were added. The Recorder Data Conversion tool was only used to convert data from SCADAS format to other formats. Some instructions for the Recorder Data conversion tool here: 

Download links here (requires Support Center login):

Past versions of the Recorder Tool can be downloaded here:
Other Simcenter Testlab Installation Resources:
*** Use for reading Simcenter Testlab files in Simcenter 3D, Simcenter Testlab 2306 and higher is only 64 bit

KB Article ID# KB000042893_EN_US

Contents

SummaryDetails

Associated Components

Simcenter Testlab Digital Image Correlation Testlab Environmental Testlab Acoustics Testlab Data Management Testlab Desktop Testlab Durability Testlab General Acquisition Testlab General Processing & Reporting Testlab Rotating Machinery & Engine Testlab Sound Designer Testlab Structural Dynamics Testlab Turbine