Direct YouTube link: https://youtu.be/J5Vf9msmrUk
Processing cursor for interactive order analysis...
Use the Processing cursor with a Colormap display and detached FrontBack display to view orders interactively.
First, display a waterfall data in the Simcenter Testlab Desktop Navigator worksheet (formerly called LMS Test.Lab).
![colormap1.png colormap1.png](media/0EM4O00000113ht)
Picture 1: Colormap display in Simcenter Testlab Desktop Navigator worksheet
In the upper right corner near the display, click on the “Add a detached picture window” icon.
![detached.png detached.png](media/0EM4O00000113hu)
Picture 2: In the upper right corner of the display area, click on the "Add a detached picture window" button
In the newly opened detached display, add a FrontBack layout.
![colormap2.png colormap2.png](media/0EM4O00000113hv)
Picture 3: Open a FrontBack layout in the detached display.
Now right click in the colormap display and choose “Add Processing Cursor -> Order”
![colormap3.png colormap3.png](media/0EM4O00000113hw)
Picture 4: Right click on the colormap display and select "Add Processing Cursor -> Order"
From the “Cursor Processing” dialog box, drag and drop the order function to the detached Front/Back display.
![colormap4.png colormap4.png](media/0EM4O00000113hx)
Picture 5: From the "Cursor Processing" dialog box, drag and drop the order section into the FrontBack display.
Close the “Cursor Processing” dialog box by clicking on the X in the upper right corner of the dialog box.
Drag the order cursor in the colormap and to view it in the detached picture. The order cut will dynamically update as the cursor moves.
![colormap5.png colormap5.png](media/0EM4O00000113hy)
Picture 6: Move the order cursor in the colormap display to see it update in the detached picture.
Multiple Order Cursors
Multiple processing cursors can be used and overlayed in the detached display.
![colormap6.png colormap6.png](media/0EM4O00000113hz)
Picture 7: Multiple order processing cursors can be overlayed in the detached display.
Order Width
If you wish to set the order width, double click on the order cut in the “Cursor Processing” dialog.
![order_width.png order_width.png](media/0EM4O00000113i0)
Picture 8: Double click on the order section in the "Cursor Processing" dialog to set the order width.
If the cursor dialog is closed, it can be reopened by right clicking on the order cursor in the colormap and selecting “Processing…”.
![order_width2.png order_width2.png](media/0EM4O00000113i1)
Picture 9: Re-open the "Cursor Processing" dialog by right clicking on the order cursor and selecting "Processing..."
Questions? Post a reply, email peter.schaldenbrand@siemens.com, or contact Siemens Support Center.
Related Rotational Dynamics links:
Simcenter Testlab Display Tips: