Simcenter Testing Solutions Hands-Free Data Acquisition! (Almost...)

2019-08-29T16:35:21.000-0400
Simcenter Testlab

Summary


Details

overview.png

 

Taking data on the road?

Probably a good idea to keep everything as hands-free as possible. Use these four tips to keep your eyes on the road and your hands on the wheel:

USB Remote Control

Simcenter Testlab Signature (previously known as LMS Test.Lab) has built-in support for a USB remote (Product code: SCX-RC01). Use it to initiate a measurement, accept or reject data, and to perform auto-ranging. The remote control plugs into any laptop running Simcenter Testlab Signature testing.

remote.png
The Scadas remote control (SCX-RC01) in use during vehicle measurement.

After plugging the remote control into your laptop, make sure in Simcenter Testlab Signature that your activate it from the main menu by selecting “Tools -> Add-ins -> Remote Control”. Note that this remote control also works with Simcenter Test.Xpress.

Keyboard Shortcuts

Don’t have a remote? Use the keyboard on your laptop instead. In the lower right corner of Simcenter Testlab Signature testing “Measure” worksheet, there are prompts for keyboard actions for data acquisition.

To get started, press the F2 key to ARM the system.

keyboard1.png
After pressing F2, the biggest key on your laptop is all you need: the SPACEBAR. SPACEBAR will start the measurement, SPACEBAR will stop the measurement, SPACEBAR will accept data, etc.

keyboard2.png

Of course the SPACEBAR does not get all the glory! Keys like BACKSPACE are used to reject data. If you are good at taking measurements, the BACKSPACE will be a very lonely, seldom used key…

Auto-Accept

In the “Measure” worksheet of Signature testing, click on the “More…” button on the middle of the right hand side. Click on the check box next to “Automatically Accept Measurement” and press CLOSE.

auto_accept.png

Now you will NOT get an “Accept or Reject Run” message at the end of every measurement, eliminating unneeded interaction with the computer. If you need to delete data, disarm the system, and click on “Data -> Data Explorer” at the top menu. After finding the Run desired to be deleted, right click on it and choose “Delete”.

Auto-Measure

Another great setting under the “More…” button is setting the sequence length greater than the default value of “1”. For example, setting it to 10 will cause the system to take 10 acquisitions in a row.

auto_rearm.png

In the upper right corner, the system will show how many runs out of 10 that you have acquired.

sequence.png

Combined with a trigger, you could have data taken whenever a certain condition is met. For example, if the engine rpm exceed 1000 rpm, it will automatically take data up to 10 times in a row, with no user interaction. Or when exceeding 30 kph, or vibration levels exceed 2 g's, etc.

 

Enjoy! If you have questions, email scott.beebe@siemens.com or contact Siemens Support Center.

 

Simcenter Testlab Data Acquisition Tips:

Simcenter Testlab Display tips:

KB Article ID# KB000042735_EN_US

Contents

SummaryDetails

Associated Components

Simcenter Testlab Digital Image Correlation Testlab Environmental Testlab Acoustics Testlab Data Management Testlab Desktop Testlab Durability Testlab General Acquisition Testlab General Processing & Reporting Testlab Rotating Machinery & Engine Testlab Sound Designer Testlab Structural Dynamics Testlab Turbine