Simcenter Testing Solutions How to set up the Simcenter Qsources Integral Shaker

2019-08-29T16:35:35.000-0400
Simcenter Testlab Other Hardware

Summary


Details

This video demonstrates the setup preparation of the Simcenter Qsources Integral Shaker (Q-ISH).

User-added image

Video: Q-ISH Installation Instructions

The Simcenter Qsources Integral Shaker is a general use electrodynamic inertia shaker. This shaker enables Frequency Response Function (FRF) measurements in an efficient and accurate way. Typical size of structures under test range from full vehicle down to engine subcomponents of only several kilogram. The patented internal decoupling suspension of the inert mass combined with integrated force and driving point accelerometer allows to measure excite all body connection interfaces with suspension and driveline within one day. The fact the shaker does not need any alignment or external support makes that data collection for modal analysis is done very efficiently.

Questions?  Email peter.schaldenbrand@siemens.com or download the brochure attached to this article.

Related Links:

KB Article ID# KB000042694_EN_US

Contents

SummaryDetails

Associated Components

Simcenter Testlab Digital Image Correlation Testlab Environmental Testlab Acoustics Testlab Data Management Testlab Desktop Testlab Durability Testlab General Acquisition Testlab General Processing & Reporting Testlab Rotating Machinery & Engine Testlab Sound Designer Testlab Structural Dynamics Testlab Turbine