What does error message “**ERROR (Intake Valve 1): Valve head construction faces missing” mean in STAR-CCM+ In-Cylinder?

2023-01-26T02:01:40.000-0500

Summary

The present error is normally encountered during the Creation of Cylinder and Valves, if we are not assigning the correct face names to the faces of the respective Engine Part Surfaces.


Details

The error message "**ERROR (Intake Valve 1): Valve head construction faces missing"  may appear during Create Cylinder and Valves in Simcenter STAR-CCM+ In-Cylinder. This generally happens if CAD face naming does not follow the recommended best practice. To resolve this issue, you need to import the CAD model into Simcenter STAR-CCM+ 3D CAD. Then, in 3D CAD, rename the CAD faces in accordance to the standard best practice, as shown in the picture below.

User-added image

 

KB Article ID# KB000040723_EN_US

Contents

SummaryDetails

Associated Components