Simcenter STAR-CCM+ How to fix STAR-NX Error: Could not find valid CAD install

2023-01-06T04:18:41.000-0500
Simcenter STAR-CCM+ Xcelerator Share Simcenter Cloud HPC

Summary

This article outlines different reasons that cause the above error, provides hints to identify and address it.


Details

The error message "Could not find valid CAD install", appears due to the following two reasons in a windows machine:
1. Absence of the NX installation of a particular version.
2. Non-availability/creation of NX registry under Unigraphics Solutions folder, due to custom installations. 


User-added image

Fig 1: Update Model in STAR-CCM+

While executing the "Update Model" command, STAR-CCM+ starts looking for NX installation. The above error message appears If it is not found.

User-added image

To address the present error, please check if the correct version of NX is installed; there is also a need to check for the existence of NX registry under the Unigraphics Solutions folder (as shown above).
Due to custom installations, it is possible that NX registry was not created in registry under Unigraphics Solutions folder. Sometimes, it could also have been manually moved to some other location.
If either of this was not found (NX folder not created or moved to some other location), please add NX folder to its corresponding paths.

For NX 12 and below, please check the registry keys at Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Unigraphics Solutions\NX\12.x

For Simcenter 3D and NX 1847 and above please check the registry keys at Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Siemens\

Note: Typically, we don’t need to restart the machine for this change to take effect.

KB Article ID# KB000039171_EN_US

Contents

SummaryDetails

Associated Components

Design Manager Electronics Cooling In-Cylinder (STAR-ICE) Job Manager Simcenter STAR-CCM+