Simcenter STAR-CCM+ Are there any tips to speed up the parallel performance when using DEM?

2023-11-02T04:00:17.000-0400
Simcenter STAR-CCM+ Simcenter STAR-CCM+ Virtual Reality Teamcenter Share Simcenter Cloud HPC Simcenter STAR-CCM+ Viewer Simcenter STAR-CCM+ Application Specific Solutions

Summary

This article covers the considerations to be made when looking to speed up a DEM simulation.


Details

There are several different tactics to use in attempting to speed up a DEM calculation:
 

  1. Use the latest version of Simcenter STAR-CCM+; there is a continuous effort to improve the turnaround time for DEM simulations with each version. See the Spotlight On... Discrete Element Method (DEM) article for the latest version information.

  1. The number of processors should be limited by the number derived from dividing the (target) number of particles by 1500.  With the number of particles per processor less than 1500, the benefits of parallel runs are reduced.

  1. For parallel runs, enable Load Balancing feature of the Lagrangian Multiphase solver (this feature was introduced in v8.02). For parallel runs using multiple regions, always set the ‘Partitioning method’ of ‘Partitioning’ solver to ‘Per-Continuum’ (this feature was introduced in v8.04)

  1. The DEM particle time step depends on the particle density, the particle Young’s modulus and the particle size. Decreasing Young’s modulus or increasing particle size will increase the particle time step and reduce the simulation time. This does alter the problem physics but will help speed things up. For small particles, changing Young’s modulus will not have a significant effect in all likelihood.

  1. Activate the Lagrangian and DEM solver verbosities, and look for how many substeps are taken by the DEM/L2P solver. If this number is large and/or is maxing out (default max is 20000 substeps) then stop the run and look at the parcel DEM time step. The code time step divided by the parcel DEM time step is the substep number. If large, lowering the code time step can enable the DEM solver to run faster.

 

c494 (2).png

See also:
Spotlight On... Discrete Element Method (DEM) (*)
Tips and Tricks: Exploring DEM in Simcenter STAR-CCM+ (*)
How to Set Up DEM Physics (*)
Things to take into account for uncoupled, one-way or two-way coupled DEM simulations (*)

(*) Link only available to users with an account in our Support Center. You can find the instructions for accessing our Support Center on our YouTube Channel.

 

KB Article ID# KB000036341_EN_US

Contents

SummaryDetails

Associated Components

Design Manager Electronics Cooling In-Cylinder (STAR-ICE) Job Manager Simcenter STAR-CCM+