Simcenter Testlab Neo: Audio Replay

2019-10-24T03:22:00.000-0400

Summary


Details


Direct YouTube link: https://youtu.be/LOE5mEBV7c8



Simcenter Testlab Neo: Audio Replay

This article covers how to do audio replay in Simcenter Testlab Neo (Figure 1).  The menus reflect Simcenter Testlab Neo 2021 and higher.
 
User-added image
Figure 1: Simcenter Testlab Neo Audio Replay
 
The Audio Replay feature of Simcenter Testlab Neo allows playback from time histories and their corresponding colormaps.  Filters can be applied while listening to isolate sounds.  Different sounds can also be played back to back instantaneously through switching.

Contents:
1.    Getting Started
2.    Basic Audio Replay
3.    Replay Icons and Switching
4.    Advanced Audio Replay
   4.1 Live Spectrum
   4.2 Colormap Axes Swap
   4.3 Live Filtering 

   4.4 PWM Filter, Variable RPM Filter, and FRF Filter
5.    Segments

1. Getting Started

To use audio replay in Simcenter Testlab Neo, go to “File -> Add-ins” as shown in Figure 2:
User-added image
Figure 2: Audio replay add-ins available under “File -> Add-ins”

There are two add-ins that enable audio playback:
  • Basic Audio Replay: Enables equalized and calibrated playback with a highlighted replay trace and playback cursor. 
  • Advanced Audio Replay: Includes the basic replay functionality in addition to interactive filtering. Advanced Audio Replay requires 12 tokens. 
The features of each add-in are described in more detail in the next sections.

2.    Basic Audio Replay

With the Basic Audio Replay add-in activated, three new items appear in the menus as shown in Figure 3:

User-added image
Figure 3: With the Basic Audio Replay add-in, an Audio Replay ribbon (1) appears at the top, audio replay properties (2) on the right side, and a play button (3) in the lower left

The three items are:
  1. Audio Replay Ribbon: Allows replay device to be selected
  2. Audio Replay Properties: Key replay settings that are also available in the ribbon
  3. Audio Replay Button: Play button
Playback is initiated by using the play button in the lower left.  See the video more details on how basic audio replay works:

Direct YouTube link: https://youtu.be/iYEDjgW0TW4


To replay sound data, use the following order of operations: 
  • Press the play button in the lower left
  • Click the speaker icon (Figure 4) in the displays to play a trace 
  • Move the cursor to the desired segment for replay 
3. Replay Icons and Switching

During replay, icons appear on data that can be played back.  Icons can be used to switch back and forth during replay.  

The meaning of the icons is shown in Figure 4:
 
User-added image
Figure 4: Icons and their meaning in Simcenter Testlab Neo Audio Playback
 
NOTE: The relative volume levels of recordings are respected during playback during switching.

It is possible to select the data to replay from frequency domain data in the displays as shown in Figure 5.
 
User-added image
Figure 5: It is also possible to replay frequency-domain data (like spectrums and waterfalls) if the throughput is linked in the project
 
The replay icon appears on the colormap and just needs to be clicked, same as with time domain data.

4. Advanced Audio Replay

For more audio replay options, turn on Advanced Audio Replay (this will also automatically load Basic Audio Replay) under “File -> Add-ins”.

Advanced audio replay enables users to visualize live frequency spectrums of the audio and apply filters real time during playback.  

Two areas are added to the menus:
 
User-added image
Figure 6: The Advanced Replay icon adds live spectral icons to the ribbon (1) and filters (2)

The two features activated the Advanced Audio Replay add-in are:
  1. Live Spectrum Buttons: In the ribbon, icons appear for creating live spectral data during replay
  2. Filters: The filter area allows users to define filters to be used during replay

4.1 Live Spectrums

Clicking on the “Spectrum live” icon in the ribbon automatically creates a live frequency spectrum display that is active during replay (Figure 7).
 
User-added image
Figure 7: The “Spectrum live” button creates a frequency spectrum that is live during replay

Before a spectrum is shown, the PLAY button in the lower left must be pressed.

Click on the “Spectral Map” icon to get a live 3D dimensional colormap as shown in Figure 8.
 
User-added image
Figure 8: The ribbon icon “Spectrum map” creates a colormap display that is active during replay

Cursors will move in the map during replay. The frequency resolution of the map is set from the pulldown in the ribbon.

4.2 Colormap Swap Axes

Want to swap the time and frequency axes of the colormaps as shown in Figure 9?
 
User-added image
Figure 9: Same colormap, but with time and frequency axes swapped

To swap the axes, right click on the colormap and choose “Options”.  In the resulting menu, select “Miscellaneous” and choose ZX or XZ as needed (Figure 10).
 
User-added image
Figure 10: Swap axes of colormap under the “Miscellaneous” Tab of the colormap options
 
The frequency and time axes will be swapped in the display.

4.3 Live Filters

It is also possible to apply filters to the sound during replay as shown in Figure 11.
 
User-added image
Figure 11: Add a filter type by clicking on a button (1) and adjust the filter frequency settings with the magenta cursors (2) that appear in the display
 
In Area 1 of Figure 11, filters can be created and removed.  They can also be turned on and off as shown in Figure 12.
 
User-added image
Figure 12: Add filters, turn filters on and off, and remove filters
 
Note that all filters can be switched on and off simultaneously with the “Bypass Filters” icon in the Audio Replay ribbon.

While playing back the data, the filter frequency range can be adjusted by moving the magenta cursors in the display (Area 2 of Figure 11).

Filter types include:
  • None: No filter is applied.
  • Low pass: Frequencies below a specified cutoff frequency are passed.
  • High pass: Frequencies above a specified cutoff frequency are passed.
  • Notch: A narrow range of frequency is attenuated. The frequency and width are specified.
  • Band stop: A range (band) of frequencies are attenuated. An upper and lower frequency are specified. For a bandwidth smaller than 10Hz, it is recommended to use a notch filter instead.
  • Band pass: A range (band) of frequencies is passed. An upper and lower frequency are specified.  
  • Order stop: An order is filtered out. All other content remains. The order and width are specified.  A frequency offset can be specified to allow the filtering of PWM induced switching frequencies.
  • Order pass: Only the specified order remains. All other content is attenuated. The order and width are specified.
  • FRF Filter: A FRF (engineering units of ratio) can be selected and applied as a filter.  This allows different gains and attenuation per frequency.

4.4 PWM Filter, Variable RPM Filter, and FRF Filter


Direct YouTube link: https://youtu.be/9jxKAovcn8s

Some new features were added to live filters in  Simcenter Testlab Neo 2306 and higher:  
User-added image
Figure 13: Frequency Offset on Order Filter in Simcenter Testlab Neo Audio Replay
 
  • Variable Profile: Another enhancement to order filters is a variable profile.  Gain and attenuation values can be entered in dB versus RPM as shown in Figure 14.
User-added image
Figure 14: Variable profile gain for order filter.
 
  • FRF Filter: A What is a Frequency Response Function (FRF)? can be used as a filter.  This allows the gain to vary arbitrarily versus frequency.  The FRF must be in unitless (quantity: Ratio) in order to work.  After adding the FRF filter to the list of active filters, right click on the FRF and choose "Use as Audio Filter" as shown in Figure 15.
User-added image
Figure 15: FRF Filter in Simcenter Testlab Neo Audio Replay.


For more information about filters and orders, see the following Knowledge articles:

Questions? Email peter.schaldenbrand@siemens.com or contact Siemens Support Center.

Related Links:

KB Article ID# KB000036305_EN_US

Contents

SummaryDetails

Associated Components