Simcenter Testlab (formerly called LMS Test.Lab) Batch Reporting allows users to generate multi-page reports in an automated fashion.
To use Batch Reporting, it may be helpful to read the Knowledge Base article 'Format Based Printing' first to learn how to make a PowerPoint plot format file and set electronic PowerPoint file as the default print destination.
Turning it on
Batch reporting is included with Advanced Desktop. Turn it on under Tools -> Add-ins (Figure 1).
Figure 1: Tools -> Add-ins -> Batch Reporting
Batch reporting does not require tokens and is included standard in Simcenter Testlab Advanced Desktop. No extra license is required. Press OK after selecting Batch Reporting from the list of add-ins.
A new worksheet titled Batch Reporting appears at the bottom of the screen (Figure 2).
Figure 2: Batch Reporting worksheet
Add some data to be plotted to the Input basket and click on the Batch Reporting worksheet to open it.
Getting Started in Batch Reporting
In the batch reporting worksheet, click on the button in the upper left of the screen and select Input Basket (Figure 3).
Add some data to be plotted to the Input basket and click on the Batch Reporting worksheet to open it.
Getting Started in Batch Reporting
In the batch reporting worksheet, click on the button in the upper left of the screen and select Input Basket (Figure 3).
Figure 3: Set 'Input Basket' in 'Data Source Selection'
Press Close after selecting Input Basket as the 'Data Source Selection'.
Press the Add to List button to populate the data list area (Figure 4).
Figure 4: Add data to be batch plotted to list on left side of Batch Reporting
Next, select Load a Format button in the upper middle of the screen (Figure 5).
Figure 5: Select a format using Load a Format button
Don t have a format? Want to create a custom format? A format file can be created in Navigator with the Make Printformat button which as described in the Knowledge Base article on Format Based Printing .
After selecting the format, in the lower left of the Batch Reporting worksheet, switch Reporting from Current Group to All (Figure 6).
Figure 6: Set reporting to All for multi-page report
By selecting the All button, the Print button will create a multi-page will result, instead of a single page.
Grouping and Sorting
To use Batch Reporting, it is important to understand Grouping and Sorting .
Sorting determines the order in which data is plotted and grouped. For example, the sorting could be used to:
To start sorting add some columns to the data list area, by right clicking in the column header and selecting Select Columns (Figure 7).
Figure 7: Select Columns to enable sorting data
In the Select Columns dialog, possible columns to be shown are selected on the left side and made visible on the left (Figure 8). Some useful columns to add:
Figure 8: Select columns to be displayed
Move columns headers from Available on the left side to Selected on the right side using the arrow key. Press OK when finished selecting the columns.
After adding columns, data can be sorted. Just double click on top of the column to sort. The A, B, C indicate the order in which they have been sorted (Figure 9).
Figure 9: A, B and C indicate the order in which columns have been sorted
Data can be grouped. Data within a single group will go on one page in the final report.
Alternating light blue and white areas indicate the data groups. The current group is highlighted in bright blue (Figure 10).
Figure 10: Group size of 4, can plot Body vs Engine for X and Y directions for a single run for Order 2
Using sorting and grouping, one can control how the data appears in the report. For example, one could overlay data from different runs, for only the Y direction of the data, for different orders (Figure 11).
Figure 11: Group size of 6, different runs, different orders, same point
Sorting and grouping could also be used to plot only 2nd order, for different runs, and all directions (Figure 12).
Figure 12: Group size of 8, all 2nd order, different runs
Sorting and grouping is used to determine the order in which the data is plotted.
Drag and Drop
Drag and drop data from the data list (left side) into the PowerPoint format (right side) as shown in Figure 13. Make sure to drop and drag from within a single group.
Figure 13: Drag and drop data from within a group over to plot format.
When printing, the data from each group will be plotted to a separate page in the resulting report. Batch Reporting will go thru the data group by group, plotting the same data positions in each group.
Printing to Powerpoint
Under File -> Printing Options make sure printing to PowerPoint electronic file is enabled. Press the Print button (Figure 14) when ready to make a report.
Figure 14: Print button
After pressing Print , a multi-page report will generated. If printing to electronic Powerpoint file, the software will prompt for a destination file name and directory.
Use Save Template before exiting to be able to recall the batch reporting setup later.
Questions? Post a reply, email peter.schaldenbrand@siemens.com, or contact Siemens Support Center.
Simcenter Testlab:
Simcenter Testlab Displays: