From version 11.06, a new coordinate system can be created without leaving surface repair mode. Surface repair tools that use a coordinate system selector contain an additional button to the right of the coordinate system drop-down menu where appropriate. This button can be used to access the tool used to create a local coordinate system.
From version 11.06, a new coordinate system can be created without leaving surface repair mode. Surface repair tools that use a coordinate system selector contain an additional (Create a new local coordinate system) button to the right of the coordinate system drop-down menu where appropriate. Example selector buttons for the transform tool are shown below: