How to setup password less ssh on a Linux-to-Linux environment

2023-11-02T04:06:18.000-0400

Summary

Password less ssh is a requirement for Simcenter STAR-CCM+ Client-Server connection through SSH tunnel. This article explains the procedure to set it up in a Linux to Linux environment.


Details

Password less ssh is a requirement for Simcenter STAR-CCM+ Client-Server connection through SSH tunnel.

The procedure to set it up in a Linux-to-Linux environment is explained in the following lines. Please note that abdon, sakura and colossus are computer hostnames. If required, please replace them with your computer hostname. For Windows, please have a look at How to Set up Password-Free SSH from a Windows to a Linux Machine using Putty .
To set up password less ssh, first create a key pair without password (just keep hitting enter).
$ ssh-keygen
Generating public/private rsa key pair.
Enter file in which to save the key (/h/username/.ssh/id_rsa):
Created directory '/h/username/.ssh'.
Enter passphrase (empty for no passphrase):
Enter same passphrase again:
Your identification has been saved in /h/username/.ssh/id_rsa.
Your public key has been saved in /h/username/.ssh/id_rsa.pub.
The key fingerprint is:
fd:63:14:f0:c3:0c:84:7b:80:1c:38:cf:c8:d8:ec username@abdon
Now try to log in to the computer using ssh. The first time you do this, it will ask you to confirm that you trust the machine. On any subsequent logins, this prompt will this question will not appear.
$ssh abdon
The authenticity of host 'abdon (194.194.194.194)' can't be established.
RSA key fingerprint is 03:34:67:15:e0:64:75:16:59:58:33:2d:bd:63:fa.
Are you sure you want to continue connecting (yes/no)? yes
Warning: Permanently added 'abdon,194.193.148.159' (RSA) to the list of known hosts.
Last login: Mon Jan 17 14:05:07 2011 from sakura
$ssh abdon
Last login: Mon Jan 17 14:05:30 2011 from sakura
abdon<51>
ssh works with a private key and a public key. If the machines have different file systems (they most likely do) you need to copy your public key into the cluster (or other file system). Easy way uses ssh-copy-id
$ssh-copy-id -i .ssh/id_rsa.pub colossus
Now try logging into the machine, with ssh colossus, and check for the key in:
.ssh/authorized_keys
to make sure we have not added extra keys.

After successfully generating and copying the keys, we can now access a computer without any passwords.
$ssh colossus
Last login: Mon Jan 17 14:00:52 2011 from| naimh.london.cdadapco.com

 

KB Article ID# KB000031682_EN_US

Contents

SummaryDetails

Associated Components