How much additional computational time should I expect for each passive scalar I add to my domain?

2022-07-21T10:36:11.000-0400

Summary

When using a passive scalar, what additional computational time can be expected?


Details

Each passive scalar requires an additional transport equation to be solved. 
In the case of a single phase simulation with the k-Epsilon turbulence model, the increase in computational time is about 8% per passive scalar. 
In the case of an Eulerian two-phase simulation with the k-Epsilon turbulence model, the increase in computation time is around 3.5% per passive scalar.
 
See also Simcenter STAR-CCM+ User Guide sections:
  • Simulating Physics > Modeling Passive Scalars
  • Theory > Species and Passive Scalars > Passive Scalars Transport

KB Article ID# KB000031540_EN_US

Contents

SummaryDetails

Associated Components